EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_getRevisionNumber()

uint32_t EC_API_SLV_getRevisionNumber ( EC_API_SLV_SHandle_t *  pHandle,
uint32_t *  pRevisionNumber 
)

Get revision number.

Get revision number. Used by the Object Dictionary

Parameters
[in]pHandleEtherCAT API instance.
[out]pRevisionNumberRevision number.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint32_t revision = 0;
// the Call
revision = EC_API_SLV_getRevisionNumber(S_ecSlvApiHdl);
uint32_t EC_API_SLV_getRevisionNumber(EC_API_SLV_SHandle_t *pHandle, uint32_t *pRevisionNumber)
Get revision number.
Definition ecSlvApi_param.c:978
Definition ecSlvApiInternal.h:351
See also
EC_API_SLV_setRevisionNumber