EtherCAT SubDevice
2.03.00
Loading...
Searching...
No Matches
◆
EC_API_SLV_setSyncManErrLimit()
uint32_t EC_API_SLV_setSyncManErrLimit
(
EC_API_SLV_SHandle_t
*
pHandle
,
uint16_t
smErrorLimit
)
Set SyncManager sequence error counter limit.
Parameters
[in]
pHandle
The pointer to the EtherCAT API instance.
[in]
smErrorLimit
SM sequence error counter limit
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
EC_API_SLV_SHandle_t
* S_ecSlvApiHdl;
// the Call
retVal =
EC_API_SLV_setSyncManErrLimit
(S_ecSlvApiHdl, 0xff);
EC_API_SLV_setSyncManErrLimit
uint32_t EC_API_SLV_setSyncManErrLimit(EC_API_SLV_SHandle_t *pHandle, uint16_t smErrorLimit)
Set SyncManager sequence error counter limit.
Definition
ecSlvApi_param.c:823
EC_API_SLV_Handle
Definition
ecSlvApiInternal.h:351
Examples
ecSubDeviceCiA402.c
.
Parameter Configuration
generated by
1.9.8