EtherCAT SubDevice
2.03.00
Loading...
Searching...
No Matches
◆
EC_API_SLV_getVendorId()
uint32_t EC_API_SLV_getVendorId
(
EC_API_SLV_SHandle_t
*
pHandle
,
uint32_t *
pVendorId
)
Get device vendor ID.
Get device vendor ID. Used by the Object Dictionary
Parameters
[in]
pHandle
EtherCAT API instance.
[out]
pVendorId
Vendor ID.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t
* S_ecSlvApiHdl;
uint32_t vendorId = 0;
// the Call
vendorId =
EC_API_SLV_getVendorId
(S_ecSlvApiHdl);
EC_API_SLV_getVendorId
uint32_t EC_API_SLV_getVendorId(EC_API_SLV_SHandle_t *pHandle, uint32_t *pVendorId)
Get device vendor ID.
Definition
ecSlvApi_param.c:878
EC_API_SLV_Handle
Definition
ecSlvApiInternal.h:351
See also
EC_API_SLV_setVendorId
Examples
EtherCAT_SubDevice_CiA402.c
,
EtherCAT_SubDevice_Simple.c
, and
EtherCAT_SubDevice_Webserver.c
.
Parameter Configuration
generated by
1.9.8