EtherCAT SubDevice
2.03.00
Loading...
Searching...
No Matches
◆
EC_API_SLV_getHwVersion()
uint32_t EC_API_SLV_getHwVersion
(
EC_API_SLV_SHandle_t
*
pHandle
,
char **
ppHwVersion
)
Get serial number.
Get serial number. Used by the Object Dictionary
Parameters
[in]
pHandle
EtherCAT API instance.
[out]
ppHwVersion
Hardware version.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
EC_API_SLV_SHandle_t
* S_ecSlvApiHdl;
char
* hwVersion = NULL;
// the Call
hwVersion =
EC_API_SLV_getHwVersion
(S_ecSlvApiHdl);
EC_API_SLV_getHwVersion
uint32_t EC_API_SLV_getHwVersion(EC_API_SLV_SHandle_t *pHandle, char **ppHwVersion)
Get serial number.
Definition
ecSlvApi_param.c:1229
EC_API_SLV_Handle
Definition
ecSlvApiInternal.h:351
See also
EC_API_SLV_setHwVersion
Parameter Configuration
generated by
1.9.8