EtherCAT SubDevice
2.03.00
Loading...
Searching...
No Matches
◆
EC_API_SLV_postSeqOutputPDBuffer()
uint32_t EC_API_SLV_postSeqOutputPDBuffer
(
EC_API_SLV_SHandle_t
*
pHandle
,
uint32_t
length
,
void *
pData
)
Release Rx Buffer.
Parameters
[in]
pHandle
pointer to API instance.
[in]
pData
Send allocated buffer.
[in]
length
length of buffer
Returns
error code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t
* pHandle;
// the Call
retVal =
EC_API_SLV_postSeqOutputPDBuffer
(pHandle);
EC_API_SLV_postSeqOutputPDBuffer
uint32_t EC_API_SLV_postSeqOutputPDBuffer(EC_API_SLV_SHandle_t *pHandle, uint32_t length, void *pData)
Release Rx Buffer.
Definition
ecSlvApi_pdo.c:2697
EC_API_SLV_Handle
Definition
ecSlvApiInternal.h:351
See also
EC_API_SLV_postSeqInputPDBuffer
Examples
ESL_cia402Demo.c
.
Buffer Handling API
generated by
1.9.8