EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_postSeqInputPDBuffer()

uint32_t EC_API_SLV_postSeqInputPDBuffer ( EC_API_SLV_SHandle_t *  pHandle,
uint32_t  length,
void *  pData 
)

Release Tx Buffer.

Parameters
[in]pHandlepointer to API instance.
[in]pDataSend allocated buffer.
[in]lengthlength of buffer
Returns
error code
Example
#include <ecSlvApi.h>
// required variables
void* pvBuffer;
// the Call
retVal = EC_API_SLV_postSeqInputPDBuffer(pHandle, pvBuffer);
uint32_t EC_API_SLV_postSeqInputPDBuffer(EC_API_SLV_SHandle_t *pHandle, uint32_t length, void *pData)
Release Tx Buffer.
Definition ecSlvApi_pdo.c:2648
Definition ecSlvApiInternal.h:351
See also
EC_API_SLV_preSeqInputPDBuffer
Examples
ESL_cia402Demo.c.