EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_run()

uint32_t EC_API_SLV_run ( EC_API_SLV_SHandle_t *  pHandle)

This is the function to run the EtherCAT Slave API.

If a adapter was initialized it can then run with this function. Fieldbus communication starts with this function

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
EC_API_EError_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_run(S_ecSlvApiHdl);
uint32_t EC_API_SLV_run(EC_API_SLV_SHandle_t *pHandle)
This is the function to run the EtherCAT Slave API.
Definition ecSlvApi.c:1455
enum EC_API_EError EC_API_EError_t
Definition ecSlvApiInternal.h:351
See also
EC_API_SLV_init, EC_API_SLV_stop
Examples
ecSubDeviceCiA402.c, and ecSubDeviceSimple.c.