EtherCAT SubDevice
2.03.00
Loading...
Searching...
No Matches
◆
EC_API_SLV_getSendMbxSize()
uint32_t EC_API_SLV_getSendMbxSize
(
uint16_t *
mailboxSize
)
Function to get configured send mailbox size (syncManager1 size).
Parameters
[out]
mailboxSize
configured send mailbox size.
Returns
ErrorCode API Error Code.
Example
#include <ecSlvApi_base.h>
// required variables
uint32_t retVal = 0;
uint16_t mbxSize = 0;
// the Call
retVal =
EC_API_SLV_getSendMbxSize
(&mbxSize);
EC_API_SLV_getSendMbxSize
uint32_t EC_API_SLV_getSendMbxSize(uint16_t *mailboxSize)
Function to get configured send mailbox size (syncManager1 size).
Definition
ecSlvApi.c:2841
Basic Functions
generated by
1.9.8