EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_writeByteEscRegister()

uint32_t EC_API_SLV_writeByteEscRegister ( EC_API_SLV_SHandle_t *  pHandle,
uint16_t  escAddress,
uint8_t  value 
)

Write to virtual ESC register.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]escAddressThe ESC Address
[in]valueNew value
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
uint8_t alEscCtrlStatus = 8;
// the Call
EC_API_SLV_writeByteEscRegister(pHandle, 0x120, alEscCtrlStatus);
uint32_t EC_API_SLV_writeByteEscRegister(EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint8_t value)
Write to virtual ESC register.
Definition ecSlvApi.c:2227