EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_cbRegisterMeasurement()

uint32_t EC_API_SLV_cbRegisterMeasurement ( EC_API_SLV_SHandle_t *  pHandle,
EC_API_SLV_CBMsrmt_t  cbFunc,
void *  pContext 
)

Register measurement callback.

Parameters
[in]pHandleSlave API Handle Instance
[in]cbFuncMeasurement Callback
[in]pContextflashInit call context
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
// the Call
EC_API_SLV_cbRegisterMsrmtHandler(pHandle, cbFunc, pCtxt);
void(* EC_API_SLV_CBMsrmt_t)(void *pMsrmtCtxt, uint32_t measureChannel, bool channelOn)
Called on severe Stack error (OSAL_error)
Definition ecSlvApi_types.h:242
Definition ecSlvApiInternal.h:351
Examples
ecSubDeviceCiA402.c.