EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_getReceiveMbxSize()

uint32_t EC_API_SLV_getReceiveMbxSize ( uint16_t *  mailboxSize)

Function to get configured receive mailbox size (syncManager0 size).

Parameters
[out]mailboxSizeconfigured receive mailbox size.
Returns
ErrorCode API Error Code.
Example
#include <ecSlvApi_base.h>
// required variables
uint32_t retVal = 0;
uint16_t mbxSize = 0;
// the Call
retVal = EC_API_SLV_getReceiveMbxSize(&mbxSize);
uint32_t EC_API_SLV_getReceiveMbxSize(uint16_t *mailboxSize)
Function to get configured receive mailbox size (syncManager0 size).
Definition ecSlvApi.c:2797