The basic API functions cover general functionality such as creating, initializing, starting, and deleting an EtherCAT subdevice object. The subdevice object is a required input parameter for all other subdevice API functions. Also supported are API functions to retrieve the subdevice status and to register status and error handler callback functions.
Functions | |
| uint32_t | EC_API_SLV_getVersion (EC_API_SLV_SHandle_t *pHandle, uint32_t *pVersion) |
| Get Stack Library Version. | |
| uint32_t | EC_API_SLV_getVersionStr (EC_API_SLV_SHandle_t *pHandle, uint32_t bufLen, char *pBuffer, uint32_t *pUsedLen) |
| Get version string. | |
| uint32_t | EC_API_SLV_getVersionId (EC_API_SLV_SHandle_t *pHandle, uint32_t bufLen, char *pBuffer, uint32_t *pUsedLen) |
| Get Version Id (Shasum) | |
| uint32_t | EC_API_SLV_stackInit (void) |
| This is the function to initialize Stack backend. | |
| EC_API_SLV_SHandle_t * | EC_API_SLV_new (void) |
| This is the function to create a new EtherCAT Slave device instance. | |
| uint32_t | EC_API_SLV_delete (EC_API_SLV_SHandle_t *pHandle) |
| This is the function to delete a created adapter. | |
| uint32_t | EC_API_SLV_init (EC_API_SLV_SHandle_t *pHandle) |
| This is the function to initialize the EtherCAT Slave API. | |
| uint32_t | EC_API_SLV_run (EC_API_SLV_SHandle_t *pHandle) |
| This is the function to run the EtherCAT Slave API. | |
| uint32_t | EC_API_SLV_stop (EC_API_SLV_SHandle_t *pHandle) |
| This is the function to stop the EtherCAT Slave API. | |
| uint32_t | EC_API_SLV_reset (EC_API_SLV_SHandle_t *pHandle) |
| Reset configuration to default values. | |
| uint32_t | EC_API_SLV_getConfigStatus (EC_API_SLV_SHandle_t *pHandle) |
| This function reads the EtherCAT driver status. | |
| uint32_t | EC_API_SLV_getCyclicStatus (EC_API_SLV_SHandle_t *pHandle) |
| This function reads if there is any error cyclic communication error. | |
| uint32_t | EC_API_SLV_getState (EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_EEsmState_t *pState, uint16_t *pAlErrorCode) |
| This is the function to read the EtherCAT Slave state machine. | |
| uint32_t | EC_API_SLV_setState (EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_EEsmState_t state, uint16_t alErrorCode) |
| This is the function to request a EtherCAT state. | |
| uint32_t | EC_API_SLV_setStationAlias (EC_API_SLV_SHandle_t *pHandle, uint16_t stationAlias) |
| This is the function to set station alias. | |
| uint32_t | EC_API_SLV_readByteEscRegister (EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint8_t *pValue) |
| This is the function reads a byte from ESC Register. | |
| uint32_t | EC_API_SLV_readWordEscRegister (EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint16_t *pValue) |
| This is the function reads a byte from ESC Register. | |
| uint32_t | EC_API_SLV_readDoubleWordEscRegister (EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint32_t *pValue) |
| This is the function reads a byte from ESC Register. | |
| uint32_t | EC_API_SLV_writeByteEscRegister (EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint8_t value) |
| Write to virtual ESC register. | |
| uint32_t | EC_API_SLV_writeWordEscRegister (EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint16_t value) |
| Write to virtual ESC register. | |
| uint32_t | EC_API_SLV_writeDoubleWordEscRegister (EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint32_t value) |
| Write to ESC register. | |
| uint32_t | EC_API_SLV_mainLoopCyclic (void) |
| Trigger stack mainloop. | |
| uint32_t | EC_API_SLV_cbRegisterErrorHandler (EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_CBStackError_t cbFunc, void *pContext) |
| Register Error callback handler. | |
| uint32_t | EC_API_SLV_enableMdioManualMode (EC_API_SLV_SHandle_t *pHandle, uint32_t manualMdioAddress, uint32_t firmwareConfig) |
| Enable mdio manual mode (TI workaround enable) | |
| uint32_t | EC_API_SLV_cbRegisterMeasurement (EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_CBMsrmt_t cbFunc, void *pContext) |
| Register measurement callback. | |
| uint32_t | EC_API_SLV_getReceiveMbxSize (uint16_t *mailboxSize) |
| Function to get configured receive mailbox size (syncManager0 size). | |
| uint32_t | EC_API_SLV_getSendMbxSize (uint16_t *mailboxSize) |
| Function to get configured send mailbox size (syncManager1 size). | |