EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_CiA402_CBUsrApplSM_t

typedef bool(* EC_API_SLV_CiA402_CBUsrApplSM_t) (void *pAppRunCtxt)

User defined function. Called as "application Cia402 StateMachine" in MainLoop.

If function is not provided, the DTK uses an internal CiA402 State Machine.

Parameters
[in]pAppRunCtxtCallBack Content for use in complex applications.
Returns
bool true if statemachine handled, false handle in stack