EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_AoE_cbRegisterReadRequestHandler()

uint32_t EC_API_SLV_AoE_cbRegisterReadRequestHandler ( EC_API_SLV_SHandle_t *  pHandle,
EC_API_SLV_AoE_CBReadRequestHandler_t  cbFunc,
void *  pContext 
)

Register user application to handle AoE read requests.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]cbFuncFunction pointer to user application.
[in]pContextread request call context.
Returns
ErrorCode API Error Code
Examples
ecSubDeviceSimple.c.