EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches
ESL_cia402Demo.h

CiA 402 Callbacks Example.

CiA 402 Callbacks Example.

Author
Texas Instruments Incorporated

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

#if !(defined PROTECT_ESL_CIA402DEMO_H)
#define PROTECT_ESL_CIA402DEMO_H 1
#include <ecSlvApi.h>
#include <defines/ecSlvApiDef_error.h>
#include <defines/ecSlvApiDef.h>
#include <stdint.h>
#if (defined __cplusplus)
extern "C" {
#endif
extern uint16_t EC_SLV_APP_CIA_startInputHandler(void* ctxt, uint16_t* intMask);
extern void EC_SLV_APP_setObdValues(void* ctxt);
extern void EC_SLV_APP_cia402Application(void* ctxt);
extern void EC_SLV_APP_cia402LocalError(void* ctxt, uint16_t errorCode);
extern uint32_t EC_SLV_APP_getCiA402ObjectEntryValue(void* pAppCtxt_p, EC_API_SLV_SCoE_ObjEntry_t* pObjectEntry_p,
uint16_t length_p, uint16_t* pValue_p);
#if (defined __cplusplus)
}
#endif
#endif /* PROTECT_ESL_CIA402DEMO_H */
uint16_t EC_SLV_APP_CIA_startInputHandler(void *ctxt, uint16_t *intMask)
Get cycle time information.
Definition ESL_cia402Demo.c:537
void EC_SLV_APP_cia402Application(void *ctxt)
CiA402 Application function.
Definition ESL_cia402Demo.c:1085
void EC_SLV_APP_cia402LocalError(void *ctxt, uint16_t errorCode)
Local Error function handler.
Definition ESL_cia402Demo.c:1451
uint32_t EC_SLV_APP_getCiA402ObjectEntryValue(void *pAppCtxt_p, EC_API_SLV_SCoE_ObjEntry_t *pObjectEntry_p, uint16_t length_p, uint16_t *pValue_p)
Read CiA402 Object entry.
Definition ESL_cia402Demo.c:322
void EC_SLV_APP_setObdValues(void *ctxt)
Set default values for CiA 402 object dictionary.
Definition ESL_cia402Demo.c:480
Definition ecSlvApiInternal.h:130