AM243x INDUSTRIAL COMMUNICATIONS SDK  11.00.00
Migration Guide

Components under Industrial Communications SDK were available in MCU+ SDK 7.x and 8.x releases. The folder structure of components in Indsutrial Communications SDK is kept similar to MCU SDK folder strucutre to keep the backward compatibilty as much as possible

If you are a user of MCU+ SDK, then items listed on this page that will assist you in migration to Industrial Communications SDK.

  • The examples, drivers and PRU-ICSS firmwares for Industrial Protocols and ICSSG Enet LLD are moved MCU+ SDK to Industrial Communications SDK. Folder location changes are also shown below.

Industrial Communication Protocols

Module MCU+ SDK Folder Location Industrial Communications SDK Folder Location
MDIO WA firmware sources examples/pru_io/mdio_fw source/industrial_comms/mdio_fw
EtherCAT Beckhoff SSC Demo examples/industrial_comms/ethercat_slave_beckhoff_ssc_demo examples/industrial_comms/ethercat_slave_beckhoff_ssc_demo
EtherCAT Demo using TI Integrated Stack examples/industrial_comms/ethercat_slave_demo examples/industrial_comms/ethercat_subdevice_demo/device_profiles
Custom phy module examples/industrial_comms/example_name/customPhy examples/industrial_comms/custom_phy
IOLINK master demo sources examples/industrial_comms/iolink_master_demo examples/industrial_comms/iolink_master_demo/device
EtherCAT Stack Libraries source/commercial/industrial_comms_libs/ethercat_slave source/industrial_comms/ethercat_slave/stack/lib
EtherNet/IP Stack Libraries source/commercial/industrial_comms_libs/ethernetip_adapter source/industrial_comms/ethernetip_adapter/stack/lib
IO-Link Stack Libraries source/commercial/industrial_comms_libs/iolink source/industrial_comms/iolink/stack/lib
EtherCAT-IOLink Gateway Stack Libraries source/commercial/industrial_comms_libs/ethercat_iolink_gateway source/industrial_comms/ethercat_iolink_gateway/stack/lib
  • Industrial Communications SDK also includes AM243X MCU+ SDK under mcu_plus_sdk folder.
Note
To build MCU+ SDK examples/libraries using CCS projects, user has to add ${SDK_INSTALL_PATH}/mcu_plus_sdk to "Product discovery path" in CCS.