AM243x INDUSTRIAL COMMUNICATIONS SDK  09.02.00
IO-Link Controller Demo

Introduction

This example is an IO-Link controller application based on evaluation stack provided in the SDK. Links to important sections in the detailed documentation are provided below:

IO-Link Controller GUI Tool can be downloaded from here.

Attention
If you need to reload and run the example again, EVM power-cycle is MUST.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSG ICSSG0
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp (E1/E2 Revision)
Example folder examples/industrial_comms/iolink_master_demo