|
AM243x INDUSTRIAL COMMUNICATIONS SDK
09.01.00
|
|
Go to the documentation of this file.
38 #ifndef RED_HSR_HANDLE_H_
39 #define RED_HSR_HANDLE_H_
47 #include <kernel/dpl/ClockP.h>
48 #include <kernel/dpl/TaskP.h>
54 typedef struct hsrPrp_Config_s
ClockP_Object redPruCheckTimer
Definition: hsrPrp_handle.h:71
struct ICSS_EMAC_Config_s * ICSS_EMAC_Handle
Alias for ICSS EMAC Handle containing base addresses and modules.
Definition: icss_emac.h:467
ClockP_Object redLifeCheckTimer
Definition: hsrPrp_handle.h:73
Node Table Entry.
Definition: hsrPrp_red_common.h:493
RED_INDEX_ARRAY_ENTRY * indexArrayBase
Definition: hsrPrp_handle.h:85
Bin array Entry.
Definition: hsrPrp_red_common.h:481
SemaphoreP_Object redLifeCheckSemaphore
Definition: hsrPrp_handle.h:81
TaskP_Object hsrPrpNodetableRefreshTask
Definition: hsrPrp_handle.h:79
ICSS_EMAC_Handle icssEmacHandle
Definition: hsrPrp_handle.h:65
uint32_t redPruCheckTimerNodeTableClear
Definition: hsrPrp_handle.h:69
hsrPrp_Config Structure storing the global variables
Definition: hsrPrp_handle.h:55
SemaphoreP_Object nodesTableSemaphore
Definition: hsrPrp_handle.h:83
uint32_t redPruCheckTimerHostTableFlag
Definition: hsrPrp_handle.h:67
struct hsrPrp_Config_s hsrPrpHandle
Definition: hsrPrp_handle.h:92
uint16_t supSeqNr
Definition: hsrPrp_handle.h:59
RED_FRAME * redSupFrame
Definition: hsrPrp_handle.h:75
int * num_of_collision_occured
Definition: hsrPrp_handle.h:63
RED_BIN_ARRAY_ENTRY * binArrayBase
Definition: hsrPrp_handle.h:87
int * collision_pkt_dropped
Definition: hsrPrp_handle.h:61
Definition: hsrPrp_red_common.h:146
RED_NODE_TABLE_ENTRY * nodeTableBase
Definition: hsrPrp_handle.h:89
Index array Entry.
Definition: hsrPrp_red_common.h:467
uint16_t redSeqNr
Definition: hsrPrp_handle.h:57
TaskP_Object redSupTask
Definition: hsrPrp_handle.h:77