AM243x INDUSTRIAL COMMUNICATIONS SDK  09.01.00
Release Notes 09.01.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
For release notes of MCU+ SDK, please refer to AM243X MCU+ SDK Release Notes 09.01.00.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless noted otherwise, the SW modules would work on all supported EVMs

New in this Release

Feature
Refactoring of EtherCAT API
Improvements in Discrete I/O Device example
Ethernet IP Conformance Tool v20 Support
ICSSM Ethernet/IP FW supports additional MAC address for traffic routing
IOLINK Improvements - Added NVRAM support for AM243 LP and EVM in example app. Support for flexible Maximum number of Ports
Moved ICSSG ENET LLD examples back to MCU SDK
Bug Fixes

Device and Validation Information

SOC Supported CPUs Boards Host PC
AM243x R5F AM243x GP EVM (referred to as am243x-evm in code),
AM243x LAUNCHPAD (referred to as am243x-lp in code)
Windows 10 64b or Ubuntu 18.04 64b

Tools, Compiler and Other Open Source SW Module Information

Tools / SW module Version
Code Composer Studio 12.5.0
SysConfig 1.18.0, build 3266
TI ARM CLANG 3.2.0.LTS
MCU+ SDK 9.1.0
Attention
TI ARM CLANG 3.2.0.LTS is not part of CCS by default, Follow steps at TI CLANG Compiler Toolchain to install the compiler.

Key Features

Profinet Device Stack and example. For more information, see Profinet Stack Transition

Fixed Issues

ID Head Line Module Applicable Releases Resolution/Comments
PINDSW-5668 HSR/PRP is not functional in rgmii mode HSR-PRP 08.04.00
PINDSW-5669 Read access for 0x0984 Register not enabled EtherCAT Device 08.06.00
PINDSW-5675 HSR/PRP - PTP Device is unable to keep offset under 1000 ns HSR-PRP 08.04.00
PINDSW-6644 EtherCAT - Disable Link Polling Mode Support in MDIO Workaround firmware EtherCAT Device 08.06.00
PINDSW-6904 Change of IP configuration does not work EtherNet/IP Adapter 09.00.00
PINDSW-7099 Reg.0x805.bit1 remains 0 and does not change EtherCAT Device 08.05.00

Known Issues

ID Head Line Module Applicable Releases Workaround
PINDSW-5122 DLR does not work in RGMII mode EtherNet/IP Adapter 08.04.00
PINDSW-5508 Observed "tcp_err_handler: Connection aborted (-13) while running CTT EtherNet/IP Adapter 08.06.00
PINDSW-5666 EtherNet/IP : PTP Device is unable to keep offset under 1000 ns EtherNet/IP Adapter 08.04.00 Value of OFFSET_THRESHOLD_FOR_RESET is set to 10000 ns by default in SDK
PINDSW-6587 EtherCAT syscfg - Rx MLINK enable does not enables MLINK if it is disabled from application EtherCAT Device 08.06.00

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

Examples

Module Affected API Change Additional Remarks
EtherCAT Device Refer Ethercat Example documentation Refer Ethercat Example documentation

Drivers

Module Affected API Change Additional Remarks