|
AM243x MCU+ SDK
09.00.00
|
|
Go to the documentation of this file.
51 #ifndef SDL_IP_PBIST_H_
52 #define SDL_IP_PBIST_H_
62 #include <sdl/sdl_esm.h>
64 #define PBIST_MAX_NUM_RUNS 2
uint32_t RAMT
Definition: sdl_ip_pbist.h:165
Definition: sdlr_pbist.h:53
volatile uint32_t doneFlag
Definition: sdl_ip_pbist.h:256
uint32_t I0
Definition: sdl_ip_pbist.h:149
int32_t SDL_PBIST_checkResult(const SDL_pbistRegs *pPBISTRegs, bool *pResult)
PBIST check result.
uint32_t I1
Definition: sdl_ip_pbist.h:153
uint64_t scrambleValue
Definition: sdl_ip_pbist.h:93
SDL_ESM_Inst esmInst
Definition: sdl_ip_pbist.h:254
uint32_t I2
Definition: sdl_ip_pbist.h:157
uint32_t CMS
Definition: sdl_ip_pbist.h:141
SDL_PBIST_configNeg PBISTNegConfigRun
Definition: sdl_ip_pbist.h:257
uint64_t memoryGroupsBitMap
Definition: sdl_ip_pbist.h:89
int32_t SDL_PBIST_releaseTestMode(SDL_pbistRegs *pPBISTRegs)
PBIST Release Test mode.
uint32_t CSR
Definition: sdl_ip_pbist.h:145
This structure contains the different configuration used for PBIST.
Definition: sdl_ip_pbist.h:75
uint32_t CL3
Definition: sdl_ip_pbist.h:137
uint32_t CA2
Definition: sdl_ip_pbist.h:117
SDL_pbistRegs * pPBISTRegs
Definition: sdl_ip_pbist.h:250
This file contains the SoC-specific SDL PBIST API's and definitions.
uint32_t CA1
Definition: sdl_ip_pbist.h:113
uint32_t CL0
Definition: sdl_ip_pbist.h:125
uint32_t CA0
Definition: sdl_ip_pbist.h:109
int32_t SDL_PBIST_start(SDL_pbistRegs *pPBISTRegs, const SDL_PBIST_config *pConfig)
PBIST Start.
uint32_t CL2
Definition: sdl_ip_pbist.h:133
Definition: sdl_ip_pbist.h:248
uint32_t esmEventNumber
Definition: sdl_ip_pbist.h:255
uint32_t interruptNumber
Definition: sdl_ip_pbist.h:253
uint32_t algorithmsBitMap
Definition: sdl_ip_pbist.h:85
int32_t SDL_PBIST_softReset(SDL_pbistRegs *pPBISTRegs)
PBIST Soft reset.
uint32_t CA3
Definition: sdl_ip_pbist.h:121
uint64_t PBISTRegsHiAddress
Definition: sdl_ip_pbist.h:249
uint32_t CL1
Definition: sdl_ip_pbist.h:129
This structure contains the different configuration used for PBIST for the failure insertion test to ...
Definition: sdl_ip_pbist.h:106
uint32_t I3
Definition: sdl_ip_pbist.h:161
int32_t SDL_PBIST_startNeg(SDL_pbistRegs *pPBISTRegs, const SDL_PBIST_configNeg *pConfig)
PBIST Failure Insertion Test Start.
uint32_t numPBISTRuns
Definition: sdl_ip_pbist.h:251
#define PBIST_MAX_NUM_RUNS
Definition: sdl_ip_pbist.h:64