AM243x MCU+ SDK  09.00.00
Migration Guides

Some TI SOCs offer the Processor SDK RTOS package for developing application on the RTOS/NORTOS CPUs. If you are a user of Processor SDK RTOS, the references listed on this page point to information that will assist you in migration to MCU+ SDK.

This page also contains information regarding migration between GP and HS_FS devices.

  1. Change list between Processor SDK RTOS and MCU+ SDK, see this XLS
  2. OS Kernel
    1. FreeRTOS comparison with SysBIOS, see FreeRTOS
    2. OSAL Migration Guide
  3. Bootloader
    1. Bootflow Migration Guide
  4. SOC Peripheral Drivers
    1. DDR Migration Guide
    2. GPIO Migration Guide
    3. I2C Migration Guide
    4. IPC and Mailbox Migration Guide
    5. Linker Command File Migration Guide
    6. MCSPI Migration Guide
    7. OSPI Migration Guide
    8. PINMUX Migration Guide
    9. UART Migration Guide
    10. UDMA Migration Guide
  5. Networking
  6. Device Type
    1. HS FS Migration Guide