AM243x MCU+ SDK  09.00.00
SA2UL PKA RSA Signing and Verification Test

Introduction

This example demonstrates the SA2UL PKA RSA Signing and Verification operations.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am243x-evm, am243x-lp
Example folder examples/security/crypto/sa2ul_pka/rsa_signing_verification/rsa_signing_verification.c

Steps to Run the Example

See Also

PKA

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

[PKA] RSA Signing and Verification example started ...
[PKA] RSA Signing and Verification example completed!!
All tests have passed!!