AM243x INDUSTRIAL COMMUNICATIONS SDK  09.00.00
Networking

Overview

Advances in automated factories and smart vehicles require advanced networking capabilities, real-time processing and more advanced motor-control topologies. TI Networking solution packaged with the SDK provide a rapidly growing need for Sitara MCU to out space traditional MCUs and deliver processor-like capabilities. Networking is a broad terms used to cover Ethernet (IEEE 802.3), EtherCAT Profinet and other ethernet-like communication protocols used in industrial, automotive and other general use cases. However, this document refers only onIEEE 802.3 standard Ethernet gigabit speed packet communication.

Figure: Industrial And Automotive Networking Applications

This document covers driver software architecture, Application Programming Interfaces (API), protocol stack usage, LwIP (Light Weight IP stack), examples and demos that are packaged in the SDK. The out-of-box Ethernet (CPSW) Examples enables fast on-board and accelerates the development cycle. This document also provides API guide for low level Ethernet, Industrial communication protocols drivers along with Layer-2 (low level) examples to enable advanced users to integrate the custom stack.

Networking is supported using following two hardware Peripherals:

  • Common Port SWitch (CPSW) : CPSW subsystem provides IEEE 802.3 standard Ethernet gigabit speed packet communication for the device and can also be configured as an Ethernet switch. CPSW supports RGMII and RMII Interfaces.
  • Programmable Real-Time Unit and Industrial Communication Subsystem - Gigabit (PRU-ICSSG) : PRU-ICSSG (simply refered as ICSSG) is firmware programmable and can take on various personalities like Industrial Communication Protocol Switch (for protocols like EtherCAT, Profinet, EtherNet/IP), Ethernet Switch, Ethernet MAC, Industrial Drives, etc. PRU-ICSSG supports RGMII and MII modes. This document concentrates only on IEEE 802.3 standard Ethernet gigabit speed packet communication.

To know more about the hardware peripherals, please refer to datasheet and Technical Reference Manual (TRM) on the product page:

Salient Features

Figure: Networking Software Features

Software Components Overview

Below is the software components overview highlighting mainly the components used in the Networking software development.

Figure: Networking Software Components Overview

Examples and Demos

You can find out-of-box examples and demos here.

Driver

There are separate drivers based on the use-case :

Enet LLD

Ethernet Low-Level Driver is a driver that aims at providing an unified interface for standard Ethernet MAC and switch using CPSW and PRU-ICSSG Peripherals.

ICSS-EMAC

Industrial Communications Subsystem Ethernet Media Access Controller (ICSS-EMAC) driver provide APIs to transmit and receive packets with a firmware based Ethernet switch that has been implemented on PRU-ICSS cores. It is used for 100M Industrial Ethernet Protocols like EtherNet/IP, Profinet etc.

ICSS TimeSync

ICSS TimeSync is a separate driver based on ICSS-EMAC, which provides APIs for PTP/1588 v2 receiver implementation on PRU-ICSSG.