AM243x INDUSTRIAL COMMUNICATIONS SDK  09.00.00
EtherNet/IP Adapter Demos

Introduction

These examples are EtherNet/IP Adapter applications based on evaluation stacks provided in the SDK. Links to important sections in the detailed documentation are provided below:

Attention
If you need to reload and run the example again, EVM power-cycle is MUST.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSG ICSSG1
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp (E1/E2 Revision)
Example folder examples/industrial_comms/ethernetip_adapter_demo