The Sitaraâ„¢ Digital Control Library (DCL) provides a suite of robust software functions for developers of digital control applications using the Texas Instruments Sitara MCU. DCL is a header-only library, and all functions in the library are provided in the form of C source-code.
The DCL contains PI,PID and "Direct Form" controller types. The former are typically used to tune properties of a transient response, while the latter are typically used to shape the open loop frequency response.
In addintion, DCL contains functions to convert controller parameters from one type to the other. As well as functions to parameterize the controller given a transfer function.
Several utility modules such as error handling, data logging are also included as a supporting module.
Supported controller modules (floating-point)
Other utility modules:
(Compared with C2000Ware's DCL)
A benchmark on R5F core has been conducted to observe the following results when running controller arithmetic:
| Controller Function | Cpu Cycles |
|---|---|
| PI Controller | |
| DCL_runPISeries | 49 |
| DCL_runPIParallel | 50 |
| DCL_runPISeriesTustin | 56 |
| DCL_runPIParallelEnhanced | 62 |
| PI2 Controller | |
| DCL_runPI2Series | 74 |
| PID Controller | |
| DCL_runPIDSeries | 65 |
| DCL_runPIDParallel | 65 |
| DF11 Controller | |
| DCL_runDF11 | 24 |
| DF13 Controller | |
| DCL_runDF13 | 43 |
| DCL_runDF13Clamp | 53 |
| DF22 Controller | |
| DCL_runDF22 | 27 |
| DCL_runDF22Clamp | 41 |
| DF23 Controller | |
| DCL_runDF23 | 29 |
| DCL_runDF23Clamp | 45 |
| PID 64bit Controller | |
| DCL_runPIDF64Series | 185 |
| DCL_runPIDF64Parallel | 174 |
The following examples has been provided to demonstrate the DCL library:
N/A