The Datalog library module commonly found in both digital control and motor-control applications. This module stores the real time values of user selctable variables. User configurable, "n" number of variables are selected by configuring "n" module inputs, iptr[0], iptr[1], ... iptr[n-1], point to the address of "n" variables. Data values are stored in datalog buffers, datalogBuff[0], datalogBuff[1], ... datalogBuff[n-1].
Number of datalog channels, buffer size and data type are configurable by user with "${SDK_INSTALL_PATH}/source/utilities/datalog/include/datalog_input.h" file update.
Datalog library module includes user configurable:
N/A
A benchmark on R5F core has been conducted to observe the following results when running the following functions:
| DATALOG Function | Cpu Cycles |
|---|---|
| Auto Trigger | |
| DATALOG_update | 68 |
| Manual Trigger | |
| DATALOG_update | 73 |
The following examples has been provided to demonstrate datalog module:
N/A