AM263x MCU+ SDK  09.01.00
enet_soc.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) Texas Instruments Incorporated 2020-23
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
40 #ifndef ENET_SOC_H_
41 #define ENET_SOC_H_
42 
43 /* ========================================================================== */
44 /* Include Files */
45 /* ========================================================================== */
46 
47 #include <stdint.h>
49 #include <include/core/enet_base.h>
50 #include <kernel/dpl/DebugP.h>
51 
52 #if defined(SOC_AM64X) || defined(SOC_AM243X)
53 #include <soc/k3/am64x_am243x/enet_soc.h>
54 #include <soc/k3/k3_soc.h>
55 #include <drivers/udma/soc/am64x_am243x/udma_soc.h>
56 #elif defined (SOC_AM273X)
57 #include <soc/am273x/enet_soc.h>
58 #elif defined(SOC_AWR294X)
59 #include <soc/awr294x/enet_soc.h>
60 #elif defined(SOC_AM263X)
61 #include <soc/am263x/enet_soc.h>
62 #elif defined(SOC_AM263PX)
63 #include <soc/am263px/enet_soc.h>
64 #elif defined(SOC_AWR2544)
65 #include <soc/awr2544/enet_soc.h>
66 #endif
67 
68 #ifdef __cplusplus
69 extern "C" {
70 #endif
71 
72 /* ========================================================================== */
73 /* Macros */
74 /* ========================================================================== */
75 
76 
82 #if ENET_CFG_IS_ON(ASSERT)
83 #if defined(__KLOCWORK__) || defined(__cplusplus)
84 #define EnetSoc_assert(cond, ...) do { if (!(cond)) abort(); } while (0)
85 #else /* !defined(__KLOCWORK__) && !defined(__cplusplus) */
86 #define EnetSoc_assert(cond, ...) \
87  do { \
88  DebugP_assert((bool)((cond))); \
89  } while (0)
90 #endif /* defined(__KLOCWORK__) || defined(__cplusplus) */
91 #else /* !ENET_CFG_IS_ON(ASSERT) */
92 #define EnetSoc_assert(cond, ...) (void)(cond)
93 #endif /* ENET_CFG_IS_ON(ASSERT) */
94 
95 
96 /* ========================================================================== */
97 /* Structures and Enums */
98 /* ========================================================================== */
99 
100 /* None */
101 
102 /* ========================================================================== */
103 /* Global Variables Declarations */
104 /* ========================================================================== */
105 
106 /* None */
107 
108 /* ========================================================================== */
109 /* Function Declarations */
110 /* ========================================================================== */
111 
119 int32_t EnetSoc_init(void);
120 
126 void EnetSoc_deinit(void);
127 
140  uint32_t instId);
141 
159 
172  uint32_t instId);
173 
181 uint32_t EnetSoc_getCoreId(void);
182 
196  uint32_t instId,
197  uint32_t coreId);
198 
206 uint32_t EnetSoc_getEnetNum(void);
207 
220  uint32_t instId);
221 
233 uint32_t EnetSoc_getClkFreq(Enet_Type enetType,
234  uint32_t instId,
235  uint32_t clkId);
236 
250  uint32_t instId,
251  uint32_t intrId);
252 
266  uint32_t instId,
267  uint32_t intrId);
268 
284 uint32_t EnetSoc_getIntrNum(Enet_Type enetType,
285  uint32_t instId,
286  uint32_t intrId);
287 
304  uint32_t instId,
305  uint32_t intrId);
306 
318 int32_t EnetSoc_getEFusedMacAddrs(uint8_t macAddr[][ENET_MAC_ADDR_LEN],
319  uint32_t *num);
320 
333  uint32_t instId,
334  Enet_MacPort macPort);
335 
353  uint32_t instId,
354  Enet_MacPort macPort,
355  EnetMacPort_Interface *mii);
367  uint32_t instId);
368 
369 /* ========================================================================== */
370 /* Deprecated Function Declarations */
371 /* ========================================================================== */
372 
373 /* None */
374 
375 #ifdef __cplusplus
376 }
377 #endif
378 
379 #endif /* ENET_SOC_H_ */
EnetSoc_getEnetNum
uint32_t EnetSoc_getEnetNum(void)
Get number of present Ethernet peripherals.
EnetSoc_getClkFreq
uint32_t EnetSoc_getClkFreq(Enet_Type enetType, uint32_t instId, uint32_t clkId)
Get SoC clock frequency.
EnetSoc_getEnetHandleByIdx
Enet_Handle EnetSoc_getEnetHandleByIdx(uint32_t idx)
Get handle of the Enet driver by its index.
EnetSoc_getDmaHandle
EnetDma_Handle EnetSoc_getDmaHandle(Enet_Type enetType, uint32_t instId)
Get handle of the DMA driver for a given Ethernet peripheral.
EnetSoc_getEnetHandle
Enet_Handle EnetSoc_getEnetHandle(Enet_Type enetType, uint32_t instId)
Get handle of the Enet driver for a given Ethernet peripheral.
EnetSoc_init
int32_t EnetSoc_init(void)
Initialize SoC layer.
EnetSoc_isCoreAllowed
bool EnetSoc_isCoreAllowed(Enet_Type enetType, uint32_t instId, uint32_t coreId)
Check if core is enable to use an Ethernet peripheral.
enet_types.h
This file contains the basic types using across the Enet driver.
EnetSoc_setupIntrCfg
int32_t EnetSoc_setupIntrCfg(Enet_Type enetType, uint32_t instId, uint32_t intrId)
Configure SoC connection of an interrupt.
Enet_MacPort
Enet_MacPort
MAC port.
Definition: enet_types.h:409
EnetSoc_getMacPortCaps
uint32_t EnetSoc_getMacPortCaps(Enet_Type enetType, uint32_t instId, Enet_MacPort macPort)
Get MAC port capability mask.
EnetSoc_getMacPortMii
int32_t EnetSoc_getMacPortMii(Enet_Type enetType, uint32_t instId, Enet_MacPort macPort, EnetMacPort_Interface *mii)
Get MAC port MII mode.
EnetSoc_releaseIntrCfg
int32_t EnetSoc_releaseIntrCfg(Enet_Type enetType, uint32_t instId, uint32_t intrId)
Release SoC connection of an interrupt.
EnetMacPort_Interface
MAC port interface.
Definition: enet_mod_macport.h:442
EnetSoc_deinit
void EnetSoc_deinit(void)
Deinitialize SoC layer.
EnetSoc_getIntrTriggerType
uint32_t EnetSoc_getIntrTriggerType(Enet_Type enetType, uint32_t instId, uint32_t intrId)
Get the interrupt trigger type of a peripheral interrupt signal.
EnetSoc_getMacPortMax
uint32_t EnetSoc_getMacPortMax(Enet_Type enetType, uint32_t instId)
Get number of MAC ports in a peripheral.
EnetSoc_getIntrNum
uint32_t EnetSoc_getIntrNum(Enet_Type enetType, uint32_t instId, uint32_t intrId)
Get the interrupt number of a peripheral interrupt signal.
EnetSoc_getCoreId
uint32_t EnetSoc_getCoreId(void)
Get core id of caller.
Enet_Type
Enet_Type
Ethernet peripheral type.
Definition: enet_types.h:199
EnetDma_Handle
struct EnetCpdma_DrvObj_s * EnetDma_Handle
Opaque handle for Enet CPDMA driver object.
Definition: enet_cpdma_types.h:86
DebugP.h
EnetSoc_getEFusedMacAddrs
int32_t EnetSoc_getEFusedMacAddrs(uint8_t macAddr[][ENET_MAC_ADDR_LEN], uint32_t *num)
Get EFused MAC addresses.
EnetSoc_isIpSupported
uint32_t EnetSoc_isIpSupported(Enet_Type enetType, uint32_t instId)
Validate IP support in SOC.
enet_base.h
This file contains the type definitions and helper macros for the Enet Peripheral interface.
ENET_MAC_ADDR_LEN
#define ENET_MAC_ADDR_LEN
MAC address length in bytes/octets.
Definition: enet_types.h:153
Enet_Handle
struct Enet_Obj_s * Enet_Handle
Ethernet driver handle.
Definition: enet_base.h:105