AM263x MCU+ SDK  09.01.00
eeprom.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
44 #ifndef EEPROM_H_
45 #define EEPROM_H_
46 
47 /* ========================================================================== */
48 /* Include Files */
49 /* ========================================================================== */
50 
51 #include <stdint.h>
52 #include <kernel/dpl/SystemP.h>
53 #include <kernel/dpl/SemaphoreP.h>
54 #include <drivers/i2c.h>
55 
56 #ifdef __cplusplus
57 extern "C" {
58 #endif
59 
60 /* ========================================================================== */
61 /* Macros & Typedefs */
62 /* ========================================================================== */
63 
68 #define EEPROM_PAGE_SIZE (256U)
69 
73 #define EEPROM_WR_BUF_SIZE (2U + EEPROM_PAGE_SIZE)
74 
76 typedef void *EEPROM_Handle;
78 typedef struct EEPROM_Config_s EEPROM_Config;
80 typedef struct EEPROM_Params_s EEPROM_Params;
81 
98 typedef int32_t (*EEPROM_OpenFxn)(EEPROM_Config *config,
99  const EEPROM_Params *params);
100 
111 typedef void (*EEPROM_CloseFxn)(EEPROM_Config *config);
112 
126 typedef int32_t (*EEPROM_ReadFxn)(EEPROM_Config *config,
127  uint32_t offset,
128  uint8_t *buf,
129  uint32_t len);
130 
144 typedef int32_t (*EEPROM_WriteFxn)(EEPROM_Config *config,
145  uint32_t offset,
146  const uint8_t *buf,
147  uint32_t len);
150 /* ========================================================================== */
151 /* Structure Declarations */
152 /* ========================================================================== */
153 
158 {
159  uint32_t driverInstance;
162  uint32_t i2cAddress;
164 };
165 
169 typedef struct EEPROM_Fxns_s
170 {
179 } EEPROM_Fxns;
180 
185 typedef struct EEPROM_Attrs_s
186 {
187  uint32_t size;
189  uint32_t pageCount;
191  uint32_t pageSize;
193 } EEPROM_Attrs;
194 
200 {
205  void *object;
207 };
208 
209 /* ========================================================================== */
210 /* Function Declarations */
211 /* ========================================================================== */
212 
221 void EEPROM_Params_init(EEPROM_Params *params);
222 
241 EEPROM_Handle EEPROM_open(uint32_t instanceId, const EEPROM_Params *params);
242 
249 
260 int32_t EEPROM_read(EEPROM_Handle handle,
261  uint32_t offset,
262  uint8_t *buf,
263  uint32_t len);
264 
278  uint32_t offset,
279  const uint8_t *buf,
280  uint32_t len);
281 
289 const EEPROM_Attrs *EEPROM_getAttrs(uint32_t instanceId);
290 
291 /* ========================================================================== */
292 /* Static Function Definitions */
293 /* ========================================================================== */
294 
295 /* None */
296 
297 /* ========================================================================== */
298 /* Internal/Private Structure Declarations */
299 /* ========================================================================== */
300 
304 typedef struct
305 {
308  uint32_t driverInstance;
311  uint32_t i2cAddress;
313  uint8_t pageWrBuf[EEPROM_WR_BUF_SIZE];
316  void *lock;
320 } EEPROM_Object;
321 
322 #ifdef __cplusplus
323 }
324 #endif
325 
326 #endif /* #ifndef EEPROM_H_ */
327 
EEPROM_Attrs
EEPROM device attributes, these are filled by SysCfg based on the device that is selected.
Definition: eeprom.h:186
EEPROM_WriteFxn
int32_t(* EEPROM_WriteFxn)(EEPROM_Config *config, uint32_t offset, const uint8_t *buf, uint32_t len)
Driver implementation to write to EEPROM using specific EEPROM driver.
Definition: eeprom.h:144
EEPROM_Params_s::driverInstance
uint32_t driverInstance
Definition: eeprom.h:159
EEPROM_Config_s::object
void * object
Definition: eeprom.h:205
EEPROM_Object::driverInstance
uint32_t driverInstance
Definition: eeprom.h:308
EEPROM_WR_BUF_SIZE
#define EEPROM_WR_BUF_SIZE
Temp write buffer to hold address offset and data for page write operation - 2 bytes for offset and r...
Definition: eeprom.h:73
EEPROM_Fxns::openFxn
EEPROM_OpenFxn openFxn
Definition: eeprom.h:171
EEPROM_Fxns::readFxn
EEPROM_ReadFxn readFxn
Definition: eeprom.h:175
EEPROM_Object::lock
void * lock
Definition: eeprom.h:316
SystemP.h
EEPROM_Config_s
EEPROM driver configuration, these are filled by SysCfg based on the device that is selected.
Definition: eeprom.h:200
EEPROM_close
void EEPROM_close(EEPROM_Handle handle)
Open EEPROM driver.
EEPROM_write
int32_t EEPROM_write(EEPROM_Handle handle, uint32_t offset, const uint8_t *buf, uint32_t len)
Write to EEPROM.
SemaphoreP.h
EEPROM_Params_s::i2cAddress
uint32_t i2cAddress
Definition: eeprom.h:162
EEPROM_Config_s::fxns
EEPROM_Fxns * fxns
Definition: eeprom.h:203
EEPROM_Attrs::pageCount
uint32_t pageCount
Definition: eeprom.h:189
EEPROM_Object::i2cHandle
I2C_Handle i2cHandle
Definition: eeprom.h:306
EEPROM_Object
EEPROM driver object - not to be used by application.
Definition: eeprom.h:305
EEPROM_ReadFxn
int32_t(* EEPROM_ReadFxn)(EEPROM_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from EEPROM using a specific EEPROM driver.
Definition: eeprom.h:126
I2C_Handle
struct I2C_Config_s * I2C_Handle
A handle that is returned from a I2C_open() call.
Definition: i2c/v0/i2c.h:175
EEPROM_Fxns::writeFxn
EEPROM_WriteFxn writeFxn
Definition: eeprom.h:177
EEPROM_getAttrs
const EEPROM_Attrs * EEPROM_getAttrs(uint32_t instanceId)
Return EEPROM attributes.
EEPROM_CloseFxn
void(* EEPROM_CloseFxn)(EEPROM_Config *config)
Driver implementation to close a specific EEPROM driver.
Definition: eeprom.h:111
EEPROM_Object::lockObj
SemaphoreP_Object lockObj
Definition: eeprom.h:318
EEPROM_Fxns::closeFxn
EEPROM_CloseFxn closeFxn
Definition: eeprom.h:173
EEPROM_Params_s
Parameters passed during EEPROM_open()
Definition: eeprom.h:158
EEPROM_Attrs::pageSize
uint32_t pageSize
Definition: eeprom.h:191
EEPROM_read
int32_t EEPROM_read(EEPROM_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from EEPROM.
EEPROM_Config_s::attrs
EEPROM_Attrs * attrs
Definition: eeprom.h:201
EEPROM_OpenFxn
int32_t(* EEPROM_OpenFxn)(EEPROM_Config *config, const EEPROM_Params *params)
Driver implementation to open a specific EEPROM driver.
Definition: eeprom.h:98
EEPROM_Params_init
void EEPROM_Params_init(EEPROM_Params *params)
Set default parameters in the EEPROM_Params_s structure.
EEPROM_Object::i2cAddress
uint32_t i2cAddress
Definition: eeprom.h:311
SemaphoreP_Object
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
EEPROM_open
EEPROM_Handle EEPROM_open(uint32_t instanceId, const EEPROM_Params *params)
Open EEPROM driver.
EEPROM_Attrs::size
uint32_t size
Definition: eeprom.h:187
EEPROM_Fxns
Driver implementation callbacks.
Definition: eeprom.h:170
i2c.h
EEPROM_Handle
void * EEPROM_Handle
Handle to the EEPROM driver returned by EEPROM_open()
Definition: eeprom.h:76