AM263x MCU+ SDK  09.01.00
Security

Introduction

Getting started

The HSM or Hardware security Module is a subsystem that acts as the secure host by offering security services to the rest of the system. TI offers HS-FS (High Security - Field Securable) as the primary device for the customers. The MCU+ SDK supports HS-FS device type for AM263x/AM263Px. It supports loading the HSM firmware (TIFS-MCU) via SBL (Secondary Boot Loader), which enables access to the hardware resources for cryptographic operations for R5FSS.

Bootloader_socLoadHsmRtFw

The SBL for AM263x/AM263Px/AM273x supports for loading firmware on the HSM. The firmware is provided in an encrypted form at source/drivers/hsmclient/soc/hsmRtImg.h. The function Bootloader_socLoadHsmRtFw sends a message to ROM and ROM loads the HSM firmware. After the HSM firmware is loaded and has done its init time operations, it sends a message to the SBL called HSM_MSG_BOOT_NOTIFY.

int main()
{
...
Drivers_open();
Bootloader_profileAddProfilePoint("Drivers_open");
DebugP_log("\r\n");
Bootloader_socLoadHsmRtFw(gHsmRtFw, HSMRT_IMG_SIZE_IN_BYTES);
Bootloader_profileAddProfilePoint("LoadHsmRtFw");
DebugP_log("Starting QSPI Bootloader ... \r\n");
...
}

HSMRt Firewall Configurations

HSMRt does the following firewall configurations. These configurations gives necessary access of various memory regions to host cores.

Note
Following configurations are done considering R5FSS0_0 as secure host 0 and R5FSS0_1 as secure host 1.
Firewall/MPU Programmable Region Num. Start Address End Address AID/privID permissions SR SW SX UR UW UX NS Debug Comments
FW HSM_SLV 0 0x44000400 0x44000800 HSM, R5FSS0_0,
R5FSS0_1
1 1 0 1 1 0 1 1 HSM MBOX region
R5->HSM queues
1 0x44000000 0x44000400 HSM, R5FSS0_0,
R5FSS0_1
1 0 0 1 0 0 1 1 HSM MBOX region
HSM->R5 queues
2 0x40020000 0x4011FFFF R5FSS0_0,
R5FSS0_1,
R5FSS1_0,
R5FSS1_1
1 0 0 1 0 0 1 1 MPU Region Space
3 0x40140000 0x4023FFFF R5FSS0_0,
R5FSS0_1,
R5FSS1_0,
R5FSS1_1
1 0 0 1 0 0 1 1 MPU Region Space
FW DTHE_SLV 0 0xCE007000 0xCE0073FF All AIDs can access 1 1 1 1 1 1 1 1 HSM AES (public context)
1 0xCE005000 0xCE0053FF All AIDs can acces 1 1 1 1 1 1 1 1 HSM SHA (public context)
2 0xCE000000 0xCEFFFFFF HSM 1 1 1 1 1 1 1 1 HSM DTHE and Crpyto
FW SCRM2SCRP0 0 0x53600000 0x53600400 HSM 1 1 1 1 1 1 1 1 Secure Asset and is protected during runtime
1 0x50000000 0x53600000 All AIDs can access 1 1 1 1 1 1 1 1 To access peripheral region master side MPU
FW SCRM2SCRP1 0 0x53600000 0x53600400 HSM 1 1 1 1 1 1 1 1 Secure Asset and is protected during runtime
1 0x50000000 0x53600000 All AIDs can access 1 1 1 1 1 1 1 1 To access peripheral region master side MPU
FW R5SS0_CORE0_AHB_MST 0 0x53600000 0x53600400 HSM 1 1 1 1 1 1 1 1 Secure Asset and is protected during runtime
1 0x50000000 0x53600000 All AIDs can access 1 1 1 1 1 1 1 1 To access peripheral region master side MPU
FW R5SS0_CORE1_AHB_MST 0 0x53600000 0x53600400 HSM 1 1 1 1 1 1 1 1 Secure Asset and is protected during runtime
1 0x50000000 0x53600000 All AIDs can access 1 1 1 1 1 1 1 1 To access peripheral region master side MPU
FW R5SS1_CORE0_AHB_MST 0 0x53600000 0x53600400 HSM 1 1 1 1 1 1 1 1 Secure Asset and is protected during runtime
1 0x50000000 0x53600000 All AIDs can access 1 1 1 1 1 1 1 1 To access peripheral region master side MPU
FW R5SS1_CORE1_AHB_MST 0 0x53600000 0x53600400 HSM 1 1 1 1 1 1 1 1 Secure Asset and is protected during runtime
1 0x50000000 0x53600000 All AIDs can access 1 1 1 1 1 1 1 1 To access peripheral region master side MPU

Resources available

By default, the access to the crypto resources are firewalled on HS-FS devices. The HSM firmware so loaded, bypasses the firewalls and makes the following crypto modules available for the R5FSS to use.

  • AES (public context)
  • SHA (public context)

This provides ability for the R5F core to be able to do the following computations:

  • AES encryption/decryption
  • SHA/HMAC hash calculation

SBL should always wait for HSM_MSG_BOOT_NOTIFY before using the crypto accelerator because HSM firmware initializes these firewalls. Failing to do so, the SBL or application may run into abort exception while accessing the MMR regions for the crypto accelerator.

Services

The TIFS-MCU firmware that gets loaded on HSM provides the variety of services. For more information refer HSM client

Modules

This page links to sub modules that enable authentication, data integrity and its confidentiality with the on-chip hardware accelarators.

The cryptographic accelarator on this device is supported via these modules in the SDK:

  • Cryptography Modules
    • DTHE (Data Transform and Hashing Engine)
      • Description of DTHE architecture and APIs available to use AES and SHA engine.
Note
EDMA support for AES and SHA will be added in future releases. Currently, the drivers only operate in CPU mode of data copy.