This example demonstrates how to operate Phase-Shifted Full Bridge(PSFB) DC/DC coverter of TIDM-02009 reference design using AM263x MCU. Peak Current Mode of Control(PCMC) technique is adopted here to control the converter.
Folder/Files | Description |
---|---|
psfbpcmc_main.c | Main function for PSFB converter testing |
psfbpcmc_hal.h | Solution hardware abstraction layer header file |
psfbpcmc_hal.c | Solution hardware abstraction layer initialization file |
psfbpcmc_settings.h | Predefined settings related header file |
psfbpcmc_user_settings.h | User configurable PSFB defines |
psfbpcmc.h | Solution header file |
psfbpcmc.c | Solution initialization file |
libraries/ | Folder with DCL & SFRA library related files |
IO_expander/ | Folder with IO_Mux configuration related files |
real_time_debug/ | Folder with real time debug related files |
targetConfigs/ | Folder with custom .ccxml file |
psfbpcmc.syscfg | Solution related SysConfig file |
setupdebugenv_allbuilds_AM263.js | Expression window parameter loading file |
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am263x-cc |
Example folder | examples/tidm-02009-dcdc |
Useful links for the application to run are provided below: