|
| void | commonTimerGenerateLowPowerDelay (USS_SW_Library_configuration *config, uint16_t delay, USS_low_power_mode_option lpmMode) |
| |
| void | commonTimerConfigureTick (USS_SW_Library_configuration *config) |
| |
| void | commonTimerConfigureDelay (USS_SW_Library_configuration *config, uint16_t compareRegister, uint16_t delay) |
| |
| void | commonTimerConfigurePeriodMeasurement (USS_SW_Library_configuration *config, uint16_t delay1, uint16_t delay2) |
| |
| void | commonTimerPeriodMeasurementClear (USS_SW_Library_configuration *config) |
| |
| void | commonTimerPeriodMeasurementEnableInterrupts (USS_SW_Library_configuration *config) |
| |
| void | commonTimerPeriodMeasurementDisableInterrupts (USS_SW_Library_configuration *config) |
| |
| void | commonTimerPeriodMeasurementStart (USS_SW_Library_configuration *config) |
| |
| void | commonTimerPeriodMeasurementWaitEvent1 (USS_SW_Library_configuration *config, USS_low_power_mode_option lpmMode) |
| |
| void | commonTimerPeriodMeasurementWaitEvent2 (USS_SW_Library_configuration *config, USS_low_power_mode_option lpmMode) |
| |
| bool | commonTimerWaitTickEvent (USS_SW_Library_configuration *config, USS_low_power_mode_option lpmMode) |
| |
| void | commonClearCCFlagStart (USS_SW_Library_configuration *config, uint16_t compareControlReg) |
| |
| void | commonTimerStart (USS_SW_Library_configuration *config) |
| |
| void | commonTimerStop (USS_SW_Library_configuration *config) |
| |
| void | commonTimerClear (USS_SW_Library_configuration *config) |
| |
| void | commonTimerEnableInterrupt (USS_SW_Library_configuration *config, uint16_t compareControlReg) |
| |
| void | commonTimerDisableInterrupt (USS_SW_Library_configuration *config, uint16_t compareControlReg) |
| |
| bool | commonTimerPollInterruptFlag (USS_SW_Library_configuration *config) |
| |
| bool | commonTimerConfigureTimer (USS_SW_Library_configuration *config) |
| |