Ultrasonic Water Meter Demo with MSP430FR6047 02_20_00_08
Release Notes
Document Revision: May 17, 2019
This Ultrasonic Water Flow Meter application is a portable and modular software designed to guide developers in the implementation and customization of their own water meter solutions.
This document is divided into the following sections:
What's New
- MSP430FR6047 USS Water Demo:
- Bug Fix:
- Fixed Volume Flow Calibration Calculation
- Fixed EVM430-FR6043 LCD Driver
- Minor bug fixes to MSP430FR6043 application to match MSP430FR6047
- Updated MSP430FR6043 IAR project to fix build configuration
- Updated MSP430FR6047 IAR project configuration to communicate with GUI
- Added IAR debug configuration file to default to MSP430 FET
- Enhancements:
- Updated CCS compiler to v8.2.0 for prebuilt binary images
- Updated Demo Project to use optimized Lobe library
- Updated Design Center configuration file for EVM430-FR6047/li>
- Known Issues:
- Clock error correction functionality has not yet been thoroughly tested in the Water Demo
- IAR Water Demo reports an algorithm error when using the optimized library version
- USS Library:
- Please check USSLib Release Notes
Revision History
02_20_00_04
- MSP430FR6047 USS Water Demo:
- Bug Fix:
- Properly accounts for DToF offset before sending DToF value to the GUI
- Enhancements:
- AbsToF DToF offset calibration
- When APPLICATION_ENABLE_ABSTOF_DTOF_OFFSET_CALIBRATION is enabled, the DToF offset update command from the GUI is ignored since the device is performing self-calibration
- Meter calibration for multiple volume flow rate ranges
- Disabled by default, can be enabled in the GUI by checking the Advanced Calibration Table button in the waveforms tab
- Interpolation correlation lookup table to enhance AbsToF accuracy
- Compatibility for transmitting debug data to multiple debug panels in the GUI
- Debug Clock Correction pre-define shows example of how to print debug data to different debug panels of the GUI
- Application migration from previous release:
- When APPLICATION_ENABLE_ABSTOF_DTOF_OFFSET_CALIBRATION is enabled, watchdog timeout is increased to account for offset calibration initialization
- Default DToF calculation option set to Option Estimate to also support high volume flow rates
- Known Issues:
- Clock error correction functionality has not yet been thoroughly tested in the Water Demo
- IAR Water Demo reports an algorithm error when using the optimized library version
- USS Library:
- Please check USSLib Release Notes
02_10_00_07
- MSP430FR6047 USS Water Demo:
- Bug Fix:
- Check envelope crossing threshold to be different than zero
- Enhancements:
- Supports library release 2.10.00.07
- Timer used for USSLib changed from TA4 to TA2
- Change error message based on timer selection for Design Center
- Update bandpass LEA filter Coefficients
- Initialize LEA temp buffer to zero
- Send clockRelative Error to Design Center when resonator calibration is enabled
- Place multi-tone memory in RAM (no impact on water demo)
- Application migration from previous release:
- Timer used for USSLib changed from TA4 to TA2 (compatible with previous release 1.40.00.01)
- Application will send clock relative error to Design Center instead of amplitude if resonator calibration is enabled
- Known Issues:
- IAR shows warning due to inconsistent declaration of USS_LEA_IFG in USS_Lib_HAL against USS_lea module. No issues expected.
- IAR shows warning due to placing of initialized memory segment. No issues expected.
- USS Library:
- Please check USSLib Release Notes
02_10_00_04
- MSP430FR6047 USS Water Demo:
- Bug Fix:
- Fix issue with hal_adc referencing incorrect vectors
- Change MCLK definition to 8Mhz instead of 16Mhz
- Update Envelope Crossing Treshold for Lobe and Hilbert Algorithms
- Report error with PLL Frequency outside valid range
- Fix problems with IAR project
- Enhancements:
- Supports library release 2.10.00.05
- Rename project from "USS GUI demo" to "MSP430FR6047 USS Water Demo"
- Add configuration LPM_EVM1 supporting EVM 1.0
- Add support for 16Mhz in hal_system
- Add definition of __EVM430_ID__ and __EVM430_VERSION__ to select EVM configuration
- Add definition of __EXTRA_VERSION__ to define extra information about firmware version
- hal_system gets clock configuration from USS Config
- Remove meter configurations from release
- Rework HMI layer to remove unnecessary depth and one-call functions. Simplify some functions which were doing overly complicated calculations
- Report different errors when GUI parameter validation fails
- Place USS config structure in a defined memory section
- Rename USS_ALG_ABS_TOF_HILB_xxx_SEARCH_RANGE to USS_ALG_ABS_TOF_xxx_SEARCH_RANGE
- Add support for additional TX pattern (disabled by default)
- Application migration from previous release:
- Application was renamed. Demo project needs to be re-imported to CCS/IAR
- New CCS/IAR project configuration added to support EVM 1.0
- Design Center must send a TX pattern of "Single Tone", otherwise the GUI will show an error
- Design Center must send an algorithm 0 or 1, otherwise the GUI will show an error
- The Design Center configuration must include the Envelope Crossing Treshold (in percentage) for both Algorithm #0 and #1, otherwise the algorithms won't work properly
- The Design Center configuration must include Negative and Positive search ranges for Algorithm #1 (not used for Algorithm #0), otherwise the algorithm won't work properly
- Application now reports signal amplitude in the Design Center Debug panel. Prototype of Testing_Update_Results was modified
- HAL files use and require new definitions __EVM430_ID__, __EVM430_VER__ to configure hardware (__FR6047_EVM__ deprecated). Project won't build without these definitions
- Application version stored in "VERSION" segment now includes __EXTRA_VERSION, __EVM430_ID__ and __EVM430_VER__. Project won't build without these definitions
- New Error packet implemented to send errors to Design Center. Some prototypes of ussDCCommandHandlers were modified
- Prototypes of functions in USSLibGUIApp changed to support new functionality
- Several lower-layer functions removed from hmi.h and made local to reduce unecessary depth
- Clock definition in HAL_System make reference to USS_userConfig.h definitons. User must make sure USS_userConfig.h has the correct clock definitions
- USS_ALG_ABS_TOF_HILB_xxx_SEARCH_RANGE in USS_userConfig.h was renamed to USS_ALG_ABS_TOF_xxx_SEARCH_RANGE
- Default MCLK definition in USS_userConfig.h was changed to 8Mhz
- Definitions in USS_App_userConfig.h changed. Functionality such as AGC calibration can be enabled in code, but controlled through the calibration interval variable
- CCS Linker file was modified to place USS_userConfig persistent arrays at top of memory. This change is not required but it's useful for debugging
- Option for additional TX sequence added. Not used for water application
- Some variables for multi-tone were placed in "RAM_Trill" memory segment requiring linker file changes. Not used for water application.
- USS Library:
- Please check USSLib Release Notes
02_10_00_03
- USS GUI demo project:
- Bug Fix:
- Fix IAR linker file pointing to wrong file
- Enhancements:
- Supports library release 2.10.00.04
02_10_00_02
- USS GUI demo project:
- Bug Fix:
- Fix default configuration to work out-of-the-box with RevA and RevB
- Fix size of gNVMemBlock
- Enhancements:
- Supports library release 2.10.00.02
- Add USS_ALG_WIN_NUM_CYCLES_DELTA to library configuration
- Rename USS_ALG_VOLUME_RATE_COMPUTATION_OPTION to USS_ALG_VOLUME_RATE_COMPUTATION_MODE
02_10_00_01
- USS GUI demo project:
- Bug Fix:
- Fix incorrect PPG duty cycle calculation
- Enhancements:
- Supports library release 2.10.00.01 with support for gas
- Add option to use gas in configuration file (not supported by project)
- Add support for Hilbert based computation
- Add design center support for computation mode using Param1 (options 0 and 1 supported)
- Add design center support for ULP bias using Param2
- Remove use of Param10 for winNumCycles
- Add design center support for envelope crossing treshold using Param8
- Add design center support for tracking range using Param9/10
01_40_00_01
- USS GUI demo project:
- Bug Fix:
- Enhancements:
- Supports library release 1.40.00.06
- Change application version scheme
- Add periodic DC Offset estimation, disabled by default
- winNumCycles updated with number of pulses
- USS_BIAS_IMPEDANCE set to 2800 by default
- Add checks for OSR, PLL Freq, Param[3:5,7]
- Rename GUI param structures and DCCommand Handler functions
- GUI shows "0.0" when result is close to zero
- Remove references to PPG prescaler
- Application released independently of library
- Remove Library version from application
01_00_01_08
- USS GUI demo project:
- Bug Fix:
- Add initalization of restartLowPowerCaptureCount configuration parameter
- Fix build error when disabling LCD
- Stop timer used by Design Center Comm when not used
- Move timer used by USS to optimize power consumption
- Disable ADC when not used
- Fix build error when disabling LCD
- Fix issue when error is detected during resonator calibration
- Removed unnecessary USS_DTC_START_ADDRESS macro from library configuration in all example projects
- Enhancements:
- Supports library release 1.40.00.03
- Updated USS_DIAGNOSTIC_MODE Library configuration from USS_diagnostics_mode_2 to USS_diagnostics_mode_0
- Add option to enable/disable SVSH
- Change high/low PPG periods to improve granularity
- Change range of transdducer frequency to >2Mhz
- Detect PLL error and reset USS module
- Add option to control muxChargePumpMode
- Add option to control bias impedance
- Updated application to reset USS module when a PLL unlock event is detected
- ULP bias configuration can be controlled using Param2 from USS Design Center
01_00_01_03
- USS GUI demo project:
- Bug Fix:
- Enhancements:
- Supports library release 1.30.00.04
- Implement resonator calibration
- Added filter coefficients for four different sampling frequencies
- Added option to enable Automatic Gain Control
01_00_01_00
- USS GUI demo project:
- Enhancement:
- External release with library 1.30.00.01
Device Support
The following families of devices are support in this release of MSP430 USS
Library:
- CCS 8.2.0
- IAR 7.10.5
- IQMath libraries for MSP430FR5xx/6xx. This library is added as part of the
release. The template project has been setup to reference the library
included in this release.
- USS Library. This library is added as part of the release. The template
project has been setup to reference the library included in this release.
This is a GA version.
Upgrade and Compatibility Information
The examples may be built with CCS or IAR.
Known Issues
N/A.
Additional Resources
For more information, visit www.ti.com.