Ultrasonic Gas Meter Demo with MSP430FR6043 02_30_00_01
Release Notes
Document Revision: February 04, 2020
This Ultrasonic Gas Flow Meter application is a portable and modular software designed to guide developers in the implementation and customization of their own gas meter solutions.
This document is divided into the following sections:
What's New
- MSP430FR6043 EVM USS Gas Demo:
- Bug Fix:
- Enhancements:
- Updated USS_userConfig.h based on USS SW Library 2.30.00.
- Added support for additional scale factor for VFR used in cases of larger pipes.
- Updated application to use background timer for accurate periodic measurements.
- Changed Design Center timer configuration from TIMER_A1 to TIMER_A2.
- Known Issues:
- Temperature estimation is not supported.
- USS Library:
- Please check USSLib Release Notes
Revision History
02_20_00_12
- MSP430FR6043 EVM USS Gas Demo:
- Bug Fix:
- Removed UPS / DNS AToF slip tracking.
- Updated additional trill pulse sequences for 1 / 2 MSPS.
- Updated GUI advanced parameter 8.to only enable / disable additional trill pulse sequence.
- Increased resonator calibrate interval to 30 for reduced power consumption.
- Disabled resonator calibration by default to match previous release.
- Enhancements:
- Updated CCS compiler to v8.2.0 for prebuilt binary images.
- USS Library:
- Please check USSLib Release Notes
02_20_00_07
- MSP430FR6043 EVM USS Gas Demo:
- USS Library:
- Please check USSLib Release Notes
Device Support
The following families of devices are support in this release of MSP430 USS
Library:
- CCS 8.2.0
- IAR Embedded Workbench 7.11.3
- IQMath libraries for MSP430FR5xx/6xx. This library is added as part of the
release. The template project has been setup to reference the library
included in this release.
- USS Library. This library is added as part of the release. The template
project has been setup to reference the library included in this release.
This is a GA version.
Upgrade and Compatibility Information
The examples may be built with CCS or IAR.
Known Issues
N/A.
Additional Resources
For more information, visit www.ti.com.