![]() |
![]() |
Document Revision: 021315.1159
This is the MSP430™ SMBus Library.
The MSP430™ SMBus Library is a royalty-free set of API's that provide support for master and slave protocols in a SMBus communication system.
This document is divided into the following sections:
The SMBus Library contains the following components.
| doc | API Guide, Users Guide, and Examples Guide |
| driverlib | MSP430™ Driverlib required for using the SMBus library with MSP4305xx_6xx devices |
| src | Library source code |
| examples | Example projects |
N/A
This release supports installation and development on Microsoft Windows Workstations.
This release is a GA version.
The examples may be built with either IAR or CCS. To build the examples navigate to example folder, select a project and
click the .eww project files for IAR or import the .projectspec file for CCS. See the SMBus Examples Guide for detailed usage instructions.
Current supported experimenters boards are found in the Device Support section of the release notes.
This is build 1.10.00.00 of MSP430™ SMBus Library
For more information, visit www.ti.com.