Speech Recognizer Project API Guide
v
|
![]() | The MinHMM API is the top-level API |
![]() ![]() | Build-time configuration parameters that specify what functions and capabilities were included when the MinHMM Library was built |
![]() ![]() | Macro definitions that the application uses to allocate memory for MinHMM |
![]() ![]() | Structures and types used in performing the tasks of the top-level user interface functions of MinHMM |
![]() ![]() | The top-level user interface functions within MinHMM |
![]() | The VAD API implements general audio activity detection based on the energy of an audio signal |
![]() ![]() | Functions of the VAD API |
![]() ![]() | Default parameter settings for the VAD API |
![]() ![]() | Enums and types used by the VAD API |