MSP-EXP430F5438 Experimenter's Board User Experience Demo v1.53.00 Texas Instruments, Inc. ******************************************************************************** Revision History ******************************************************************************** Ver 1.00 - May 2008 (D. Dang) - Initial Version Ver 1.10 - Jan 2009 - Review, documentation of code - Removal of code for production test - Additional support for MSP430EXP5438 Rev 1.x Ver 1.20 - Oct 2009 - Added support for F5438A (PMM & REF module) - Added support for use of TLV Device ID and ADC calibration values - Built with Code Composer Studio v3.2 Ver 1.30 - August 2010 (K. Enderle) - Reorganization of code - Added ADCtemp, LPM, and FFT programs - Added support for Grayscale text - PMM menu modified to enhance ease of use - Built with Code Composer Studio v4.0 Ver 1.31 - September 2010 (K. Enderle) - MSP430F5438A-only - Refactored project structure - Improved various modules such as hal_lcd - Added additonal user experience code such as an FFT demo and an ADC12 power consumption demo Ver 1.40 - May 2011 (W. Goh) - Refactored project structure to share code folder - Refactored code spacing - Fixed adc temp calculation warnings - Updated to use the latest HAL library Ver 1.40.01 - June 2011 (A. Dannenberg) - Fixed ImageHit JRE compatibility issue Ver 1.50.00 - August 2011 (W. Goh) - Added CCSv5 support. Software is not backward compatible with CCSv4. - Adding binary folder with MSP430Flasher support - Update to use 5xx/6xx core library v2.1 Ver 1.51.00 - May 2013 (E. Chen) - Fixed Code Size Limited project build error Ver 1.52.00 - Aug 2014 (E. Chen) - Fixed Code Size Limited project build error due to CCS update Ver 1.53.00 - Oct 2015 (E. Chen) - Fixed IAR project build error due to IAR linker command change ******************************************************************************** Project File Listing ******************************************************************************** | |--CCS |--MSP430F5438A.ccxml : Configuration file for MSP430F5438A |--lnk_msp430f5438a_mod.cmd: Linker file |--system_pre_init.c : Low level init to stop watchdog timer |--CCS_Code_Size_Limited |--MSP430F5438A.ccxml : Configuration file for MSP430F5438A |--lnk_msp430f5438a_mod.cmd: Linker file |--MSP-EXP430F5438_User_Experience_Lib.lib :Library file containing files excluded from code limited build |--system_pre_init.c : Low level init to stop watchdog timer |--MSP-EXP430F5438_HAL : folder containing driver files (Hardware Abstraction Layer) |--cc2500.h : header file for Chipcon CC2500 EMK or EZ430-RF daughterboard |--hal_adc.h : ADC driver header file |--hal_adc.c : ADC driver source file |--hal_board.h : Ports/Power Management/Clock System header file |--hal_board.c : Ports/Power Management/Clock System source file |--hal_buttons.h : Button driver header file |--hal_buttons.c : Button driver source file |--hal_lcd.h : LCD driver header file |--hal_lcd.c : LCD driver source file |--hal_lcd_fonts.c : ASCII font for LCD |--hal_lcd_fonts.h : ASCII font for LCD |--hal_rf.h : RF driver header file |--hal_rf.c : RF driver source file |--hal_rf_settings.h : RF settings header file |--hal_rtc.h : RTC headerfile |--hal_rtc.c : RTC source file |--hal_usb.h : USB driver header file |--hal_usb.c : USB driver source file |--hal_MSP-EXP430F5438.h : Master header file to be singly included in MSP-EXP430F5438 HAL project |--F5XX_6XX_Core_Lib : folder containing new hal files |--hal_FLASH.h : FLASH driver header file |--hal_FLASH.c : FLASH driver source file |--hal_macros.h : header containing macros |--hal_PMAP.h : PMAP driver header file |--hal_PMAP.c : PMAP driver source file |--hal_PMM.h : PMM driver header file |--hal_PMM.c : PMM driver source file |--hal_TLV.h : TLV driver header file |--hal_TLV.c : TLV driver source file |--hal_UCS.h : UCS driver header file |--hal_UCS.c : UCS driver source file |--UserExperienceDemo : folder containing User Experience Code |--5xx_ACTIVE_test.h : Active test header file |--5xx_ACTIVE_test.s43 : Assembly file for active test |--5xx_ACTIVE_test.asm : Assembly file for active test |--flashUtils.h : Flash utilities header file |--flashUtils.c : Flash utilities source file |--adcTemp.h : adcTemp header file |--adcTemp.c : Uses different adc setups to measure the temperature |--audio.h : Voice Recorder and Playback header file |--audio.c : Voice Recorder and Playback |--balanceBall.h : balanceBall header file |--balanceBall.c : Use accelerometer to control a ball on LCD |--clock.h : Analog & digital clocks header file |--clock.c : Analog & digital clocks |--FFT.h : FFT header file |--FFT.c : Performs/displays FFT of voice input |--FFT_430.h : FFT assembly header file |--FFT_430.s43 : Assembly file used to perform FFT |--FFT_430.asm : Assembly file used to perform FFT |--LPM.h : LPM header file |--LPM.c : Allows user to test various low-power modes |--menuSetting.c : Menu header file |--menuSetting.c : Menu for user settings and calibrations |--PMM.c : PMM header file |--PMM.c : Select VCORE and DCO speed in active mode |--PowerTest.h : PowerTest header file |--PowerTest.c : Select between Active and LPM tests |--usbTest.h : usbTest header file |--usbTest.c : UART USB communication with PC host |--UserExperienceGraphics.c: Contains images for lcd display |--UserExperienceGraphics.h: Contains images for lcd display |--UserExperience_F5438A.h : User experience header |--UserExperience_F5438A.c : main file, GUI, menu, and event handlers. |--IAR : Folder containing IAR Project files |--low_level_init.c : Low level init to stop watchdog timer |--lnk430F5438A_mod.xcl : Linker file |--main.c : calls UserExperience.c |--readme.txt : this file