------------Capacitive Touch Library for MSP432 and Getting Started Guide------------------ September 2015 Texas Instruments, Inc. ------------------------------------------------------------------------------------------- CONTENTS I. Library II. Firmware (Examples) III. Manifest I. Library ----------------------------------- The following files are found in the Library directory: CTS_HAL.c CTS_HAL.h CTS_Layer.c CTS_Layer.h II. Firmware (Source for Examples) ----------------------------------- The following example directories incude a main application file and configuration files structure.c/.h. These files are used with the files found in the source directory. The element definitions found in the configuration file structure.c uses a designated initializer list. This allows members to be initialized in any order and also enhances the readability of the element being initialized. This feature requires the GCC language extension found in Code Composer Studio (CCS). C99 is the default dialect found in IAR and therefore the default settings can be used. 430BOOST-SENSE1_CapTouch_MSP432P401R 430BOOST-SHARP96_CapTouch_MSP432P401R TouchProTool_Demo_UART_MSP432 III. Documentation ----------------------------------- The CTS for MSP432 Programmer's Guide explains the key components of and how to use the Capacitive Touch Software Library for MSP432. For more information on the example firmware, please refer to the MSP-EXP432P401R and Touch Pro GUI User Guides.