7 #ifndef __MSP430WARE_RAM_H__
8 #define __MSP430WARE_RAM_H__
10 #include "inc/hw_memmap.h"
12 #ifdef __MSP430_HAS_RC_FRAM__
31 #define RAM_SECTOR0 (0x00)
32 #define RAM_SECTOR1 (0x01)
33 #define RAM_SECTOR2 (0x02)
34 #define RAM_SECTOR3 (0x03)
43 #define RAM_RETENTION_MODE (0x00)
44 #define RAM_OFF_WAKEUP_MODE (RCRS0OFF0)
45 #define RAM_OFF_NON_WAKEUP_MODE (RCRS0OFF1)
107 #endif // __MSP430WARE_RAM_H__
void RAM_setSectorOff(uint8_t sector, uint8_t mode)
Set specified RAM sector off.
Definition: ram.c:21
uint8_t RAM_getSectorState(uint8_t sector)
Get RAM sector ON/OFF status.
Definition: ram.c:29