7 #ifndef __MSP430WARE_PMM_H__
8 #define __MSP430WARE_PMM_H__
10 #include "inc/hw_memmap.h"
12 #ifdef __MSP430_HAS_PMM_FRAM__
32 #define PMM_BOR_INTERRUPT PMMBORIFG
33 #define PMM_RST_INTERRUPT PMMRSTIFG
34 #define PMM_POR_INTERRUPT PMMPORIFG
35 #define PMM_SVSH_INTERRUPT SVSHIFG
36 #define PMM_LPM5_INTERRUPT PMMLPM5IFG
37 #define PMM_ALL (0xA7)
213 #endif // __MSP430WARE_PMM_H__
void PMM_clearInterrupt(uint16_t mask)
Clears interrupt flags for the PMM.
Definition: pmm.c:77
uint16_t PMM_getInterruptStatus(uint16_t mask)
Returns interrupt status.
Definition: pmm.c:84
void PMM_disableSVSH(void)
Disables the high-side SVS circuitry.
Definition: pmm.c:42
void PMM_enableSVSH(void)
Enables the high-side SVS circuitry.
Definition: pmm.c:35
void PMM_turnOnRegulator(void)
Makes the low-dropout voltage regulator (LDO) remain ON when going into LPM 3/4.
Definition: pmm.c:49
void PMM_trigBOR(void)
Calling this function will trigger a software Brown Out Rest (BOR).
Definition: pmm.c:70
void PMM_turnOffRegulator(void)
Turns OFF the low-dropout voltage regulator (LDO) when going into LPM3/4, thus the system will enter ...
Definition: pmm.c:56
void PMM_trigPOR(void)
Calling this function will trigger a software Power On Reset (POR).
Definition: pmm.c:63
void PMM_unlockLPM5(void)
Unlock LPM5.
Definition: pmm.c:89
void PMM_enableLowPowerReset(void)
Enables the low power reset. SVSH does not reset device, but triggers a system NMI.
Definition: pmm.c:21
void PMM_disableLowPowerReset(void)
Disables the low power reset. SVSH resets device.
Definition: pmm.c:28