This is 2.21.00.39 of MSPWare. MSPWare will allow you to develop your applications faster by providing all MSP430 and MSP432 related examples, documentation and software libraries in one package.
Moved driverlib code, examples and documentation into its own folder
1.40.01.44
Support for for MSP430FR5xx_6xx devices added (requires CCS 5.5+)
GRLib has been updated to version 1_10_00_00.
Capacitive Touch Software Library updated to version 1.20 (Requires CCS5.4)
1.40.01.19
In the previous MSP430ware driverlib releases, the function ADC12_B_memoryConfigure for the MSP430FR9xx devices did not enable the window comparator bit ADC12WINC and differential mode bit ADC12DIF even if the correct parameter is passed to the function. This has been fixed in this release.[Bug 3930]
There were minor comments/document update for driverlib APIs
In the previous MSP430ware driverlib releases, GPIO_interruptEdgeSelect() [MSP430F5xx_6xx family] function for Port2 sets P1IES not P2IES. This has been fixed in this release. [Bug 3357]
1.40.00.26
In the earlier versions of driverlib, the enableInterrupt API cleared the corresponding interrupt flag first and then enabled the interrupt. This behavior is changed from this release onwards. The flag is no longer cleared with the enableInterrupt APIs in the different peripherals. The user application is expected to invoke the clearInterrupt/clearInterruptFlag to clear the interrupt flags explicitely.
EUSCI API have been split into EUSCI_A and EUSCI_B. The current EUSCI based peripherals available are
EUSCI_B_I2C
EUSCI_A_SPI
EUSCI_B_SPI
EUSCI_A_UART
USCI API have been split into USCI_A and USCI_B. The current USCI-based peripherals available are
USCI_B_I2C
USCI_A_SPI
USCI_B_SPI
USCI_A_UART
The APIs in MSP430FR5xx_6xx, MSP430F5xx_6xx, MSP430FR57xx families have been updated to use C99 types
Assert stmts are disabled by default. To enable them comment out the #define NDEBUG statement in the inc/hw_types.h or inc/regaccess.h (depending on which file is available for your family)
1.30.00.15
Support for FR59xx has been added as well as separation of DriverLib by device family in order to make the library easier to use.
ASSERT statements in the driverlib source files do not work. This will be fixed in the future releases.
Comp_E examples in examplesxx_6xx_e will fail to build due to a bug in the existing device header file for versions of CCS less than CCS 5.3. To workaround this, please upgrade CCS or replace the msp430fr5969.h from the CCS5.3 release in your CCS install.
Comp_E examples in examplesxx_6xx_e will fail to build due to a bug in the existing device header file for versions of IAR5.5. To workaround this, please replace the msp430fr5969.h from deprecated430fr5xx_6xx_header_filesfrom the in your IAR5.5 install.
1.25.00.30
Update to MSP430ware and drverLib 1.20 with support for CCS 5.2.1
Installation and Usage instructions for CCS 5.2 and below when upgrading via update site
Comp_E examples will fail to build due to a bug in the existing device header file for versions of CCS less than CCS 5.3. To workaround this, please upgrade CCS or replace the msp430fr5969.h from the CCS5.3 release in your CCS install.
Update to MSP430ware and drverLib 1.20 with support for CCS 5.2.1
Upgrade and Compatibility Information
MSPWare 2.21.00.39 may be installed along any previous version of MSPWare. It will place a new directory in “C:\ti\msp\MSPWare_2.21.00.39” on Windows and a similar location on Linux and Mac OS X. The older version will stil be avilable on disk but CCS will discover and use the latest for TI Resource Explorer.
Installation and Usage
There are two methods to install MSPWare:
Installing via the Code Composer Studio (CCS) App Center
If you have CCS 6.0 or later you can install MSPWare via the CCS App Center.
Open up CCS
Click “View->CCS App Center”
Click the checkbox next to MSPWare
Then click “Install Software” in the top left corner of the app center.
Let CCS restart and discover the software. You can now use TI Resource Explorer within CCS
Installing via the Standalone Installer
If CCS is not your primary IDE or want an offline installer on hand you can download the standalone installer.
Download the standalone installer for your operating system from the MSPWare download page.
Double click to run the installer, the default installation path is discoverable by CCS
Run CCS and let it discover the MSPWare installation. You can now use TI Resource Explorer within CCS
Host Support
Supported Operating Systems:
Windows 7
Ubuntu 14.04 LTS
Mac OS X Yosemite (Beta)
Some components are not supported on all platforms. Check out the Known Issues part of the release notes for more information about what is not supported in each operating system.
Dependencies
This release requires the following other software components and tools versions to successfully function:
CCS 6.0+ for proper TI Resource Explorer functionality
Please look at the individual packages release notes to see their dependencies.
Device Support
Please look at the individual packages release notes to determine what devices they support.
Validation Information
This is a GA release of MSPWare. Please check the individual packages release notes to determine their validation information.
Known Issues
MSPWare is a collection of different packages from Texas Instruments. Some packages have not been updated to support Linux or Mac OS X Yosemite. A list of known packages that are not updated can be seen below. Please check the release notes of the individual packages for more information.
Linux Support
NFCLink
MSP-EXP430FR5969 Out of Box Experience GUI
MSP-EXP430FR5739 Out of Box Experience GUI
MSP-EXP430G2
MSP-EXPCC430RFx
eZ439-Chronos
Mac OS X Yosemite Support
NFCLink
MSP-EXP430FR5969 Out of Box Experience GUI
MSP-EXP430FR5739 Out of Box Experience GUI
MSP-EXP430G2
MSP-EXPCC430RFx
eZ439-Chronos
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. MSPWare_2_10_00_15.