Initial release of the TouchPro tool.
The TouchPro tool is a PC based tool to aid in the design and tuning of capacitive touch button(s), slider(s) and wheels(s). The tool receives and displays captouch sensor data to help the user quickly and easily evaluate, diagnose and tune button, slider and wheel designs.
Features of the Touch Pro Tool include:
• Receive real-time data from a target board, including up to ten
signals
• Points connected or bar chart display styles for viewing real-time
data waveforms
• User configurable automatic ranging or manual ranging of the y-axis
• Data recording and recall
• Print waveforms
• User selectable individual signal or multiple signal waveform display
The TouchPro installed directory contains the following components.
Tool Executable | An executable jar file named touchPro.jar and a batch file named touchPro.bat |
documents | Quick Start User guide to get started with the tool |
Com port driver | Included in the installed directory is the
RXTXSerial.dll |
examples | CCS and IAR project examples that transmit data from
target to host using big banging and UART interface |
Library | Included in the example projects are the CTS library files |
Source and header files | Included in the example projects are application
specific .c and .h source and header files |
Java Runtime Environment | JRE6 evnvironment included |
Run the installer and it will create TouchPro product and shortcuts under Texas Instruments.
This release supports installation and development on Microsoft Windows 7 Workstations.
This has been tested on Windows7 x64 and x32
versions
This is build 1.20.01.00 of TouchPro GUI.