Document Revision: 030315.1109
This is the MSP430 Graphics Library.
Graphics library provides an easy way to display text, graphics, and images on various LCD displays.
It also provides templates for adding new displays.
This document is divided into the following sections:
Added support to draw:
Please refer to the updated example projects which have been updated to use the new buttons APIs.
Core library is installed as part of MSPware Driver Library or can be download as a stand alone library.
Graphical Image Reformer Tool may be found here.
Graphical Image Reformer Tool allows you to convert an image to 2, 4, 8, 16, 256 bits per pixel and resize an image to fit on your particular display.
The Graphics Library contains the following components.
doc | API Guide and Users Guide |
drivers | MSP430 Peripheral Driver Library peripheral specific code examples |
html | Graphics Library documentation |
LCD_Drivers | LCD Driver files and templates |
MSP-EXP432P401R_GrlibExample_Grlib_Example | Graphics Library Example Code for MSP432P401R |
MSP-EXP430G2_Grlib_Example | Graphics Library Example Code for MSP430G2553 |
MSP-EXP430FR5969_Grlib_Example | Graphics Library Example Code for MSP430FR5969 |
MSP-EXP430FR4133_Grlib_Example | Graphics Library Example Code for MSP430FR4133 |
MSP-EXP430F5438_Grlib_Example | Graphics Library Example Code for MSP430F5438 |
MSP-EXP430F5529_Grlib_Example | Graphics Library Example Code for MSP430F5529 |
MSP-EXP430F5529LP_Grlib_Example | Graphics Library Example Code for MSP430F5529 Launchpad + BOOSTXL-K350SVG-S1 |
Empty_Project_MSP430F5xx_6xx_Grlib_Example | Graphics Library Example Code for MSP430F5xx_6xx using driverlib API calls |
Empty_Project_MSP430FR5xx_6xx_Grlib_Example | Graphics Library Example Code for MSP430FR5xx_6xx using driverlib API calls |
Empty_Project_MSP430F57xx_6xx_Grlib_Example | Graphics Library Example Code for MSP430F57xx using driverlib API calls |
Empty_Project_No_Driverlib_Grlib_Example | Graphics Library Example Code not using driverlib API calls |
N/A
This release supports installation and development on Microsoft Windows XP Workstations.
This release is a GA version.
The examples may be built with either IAR or CCS. To build the examples navigate to example folder, select a project and
click the .eww project files for IAR or import the .projectspec file for CCS.
Current supported eperimenters boards are found in the Device Support section of the release notes.
1317 | do not force black and white in palette |
1638 | 1BPP Edge Detection Option |
1649 | Display Image size in flash |
1863 | Open/Save File Path Memory |
1867 | Use Chris' 8BPP algorithm instead of stock Java algorithm |
1885 | Add blurring filter before image conversion into c-string |
1886 | Additional DCT option for better image compression |
1887 | Change compression options from compressed or not, to table of 3 compression options |
1888 | Add Loading screen to GUI during image generation |
This is build 2.00.00.17 of MSP430 Graphics Library
For more information, visit www.ti.com.