7 #ifndef __MSP430WARE_TIMER_A_H__
8 #define __MSP430WARE_TIMER_A_H__
10 #include "inc/hw_memmap.h"
12 #ifdef __MSP430_HAS_TxA3__
25 #include "inc/hw_memmap.h"
33 #define TIMER_A_THRESHOLD 50
294 #define TIMER_A_CLOCKSOURCE_DIVIDER_1 0x00
295 #define TIMER_A_CLOCKSOURCE_DIVIDER_2 0x08
296 #define TIMER_A_CLOCKSOURCE_DIVIDER_4 0x10
297 #define TIMER_A_CLOCKSOURCE_DIVIDER_8 0x18
305 #define TIMER_A_STOP_MODE MC_0
306 #define TIMER_A_UP_MODE MC_1
307 #define TIMER_A_CONTINUOUS_MODE MC_2
308 #define TIMER_A_UPDOWN_MODE MC_3
317 #define TIMER_A_DO_CLEAR TACLR
318 #define TIMER_A_SKIP_CLEAR 0x00
327 #define TIMER_A_CLOCKSOURCE_EXTERNAL_TXCLK TASSEL__TACLK
328 #define TIMER_A_CLOCKSOURCE_ACLK TASSEL__ACLK
329 #define TIMER_A_CLOCKSOURCE_SMCLK TASSEL__SMCLK
330 #define TIMER_A_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK TASSEL__INCLK
339 #define TIMER_A_TAIE_INTERRUPT_ENABLE TAIE
340 #define TIMER_A_TAIE_INTERRUPT_DISABLE 0x00
348 #define TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE CCIE
349 #define TIMER_A_CCIE_CCR0_INTERRUPT_DISABLE 0x00
357 #define TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE 0x00
358 #define TIMER_A_CAPTURECOMPARE_INTERRUPT_ENABLE CCIE
366 #define TIMER_A_CAPTURE_INPUTSELECT_CCIxA CCIS_0
367 #define TIMER_A_CAPTURE_INPUTSELECT_CCIxB CCIS_1
368 #define TIMER_A_CAPTURE_INPUTSELECT_GND CCIS_2
369 #define TIMER_A_CAPTURE_INPUTSELECT_Vcc CCIS_3
378 #define TIMER_A_OUTPUTMODE_OUTBITVALUE OUTMOD_0
379 #define TIMER_A_OUTPUTMODE_SET OUTMOD_1
380 #define TIMER_A_OUTPUTMODE_TOGGLE_RESET OUTMOD_2
381 #define TIMER_A_OUTPUTMODE_SET_RESET OUTMOD_3
382 #define TIMER_A_OUTPUTMODE_TOGGLE OUTMOD_4
383 #define TIMER_A_OUTPUTMODE_RESET OUTMOD_5
384 #define TIMER_A_OUTPUTMODE_TOGGLE_SET OUTMOD_6
385 #define TIMER_A_OUTPUTMODE_RESET_SET OUTMOD_7
403 #define TIMER_A_CAPTURECOMPARE_REGISTER_0 0x02
404 #define TIMER_A_CAPTURECOMPARE_REGISTER_1 0x04
405 #define TIMER_A_CAPTURECOMPARE_REGISTER_2 0x06
413 #define TIMER_A_CAPTUREMODE_NO_CAPTURE CM_0
414 #define TIMER_A_CAPTUREMODE_RISING_EDGE CM_1
415 #define TIMER_A_CAPTUREMODE_FALLING_EDGE CM_2
416 #define TIMER_A_CAPTUREMODE_RISING_AND_FALLING_EDGE CM_3
424 #define TIMER_A_CAPTURE_ASYNCHRONOUS 0x00
425 #define TIMER_A_CAPTURE_SYNCHRONOUS SCS
434 #define TIMER_A_CAPTURE_OVERFLOW COV
435 #define TIMER_A_CAPTURECOMPARE_INTERRUPT_FLAG CCIFG
443 #define TIMER_A_READ_SYNCHRONIZED_CAPTURECOMPAREINPUT SCCI
444 #define TIMER_A_READ_CAPTURE_COMPARE_INPUT CCI
453 #define TIMER_A_CAPTURECOMPARE_INPUT_HIGH 0x01
454 #define TIMER_A_CAPTURECOMPARE_INPUT_LOW 0x00
463 #define TIMER_A_OUTPUTMODE_OUTBITVALUE_HIGH OUT
464 #define TIMER_A_OUTPUTMODE_OUTBITVALUE_LOW 0x00
472 #define TIMER_A_INTERRUPT_NOT_PENDING 0x00
473 #define TIMER_A_INTERRUPT_PENDING 0x01
642 uint16_t captureCompareRegister);
661 uint16_t captureCompareRegister);
685 uint16_t captureCompareRegister,
722 uint16_t captureCompareRegister,
723 uint16_t
synchronized);
742 uint16_t captureCompareRegister);
759 uint16_t captureCompareRegister);
782 uint16_t captureCompareRegister,
783 uint8_t outputModeOutBitValue);
834 uint16_t compareRegister,
835 uint16_t compareValue);
868 uint16_t captureCompareRegister);
896 #endif // __MSP430WARE_TIMER_A_H__
void Timer_A_initContinuousMode(uint16_t baseAddress, Timer_A_initContinuousModeParam *param)
Configures Timer_A in continuous mode.
Definition: timer_a.c:28
uint16_t captureOutputMode
Definition: timer_a.h:119
uint16_t timerClear
Definition: timer_a.h:66
uint16_t synchronizeCaptureSource
Definition: timer_a.h:103
bool startTimer
Whether to start the timer immediately.
Definition: timer_a.h:68
void Timer_A_disableCaptureCompareInterrupt(uint16_t baseAddress, uint16_t captureCompareRegister)
Disable capture compare interrupt.
Definition: timer_a.c:169
uint16_t captureRegister
Definition: timer_a.h:84
void Timer_A_startCounter(uint16_t baseAddress, uint16_t timerMode)
Starts Timer_A counter.
Definition: timer_a.c:21
uint16_t clockSourceDivider
Definition: timer_a.h:184
void Timer_A_stop(uint16_t baseAddress)
Stops the timer.
Definition: timer_a.c:256
void Timer_A_clearCaptureCompareInterrupt(uint16_t baseAddress, uint16_t captureCompareRegister)
Clears the capture-compare interrupt flag.
Definition: timer_a.c:274
uint16_t compareOutputMode
Definition: timer_a.h:204
uint16_t timerClear
Definition: timer_a.h:247
uint16_t timerPeriod
Is the specified Timer_A period.
Definition: timer_a.h:144
void Timer_A_enableInterrupt(uint16_t baseAddress)
Enable timer interrupt.
Definition: timer_a.c:147
void Timer_A_clearTimerInterrupt(uint16_t baseAddress)
Clears the Timer TAIFG interrupt flag.
Definition: timer_a.c:269
uint16_t Timer_A_getCaptureCompareCount(uint16_t baseAddress, uint16_t captureCompareRegister)
Get current capturecompare count.
Definition: timer_a.c:215
Used in the Timer_A_initUpDownMode() function as the param parameter.
Definition: timer_a.h:128
uint16_t clockSource
Definition: timer_a.h:48
uint8_t Timer_A_getSynchronizedCaptureCompareInput(uint16_t baseAddress, uint16_t captureCompareRegister, uint16_t synchronized)
Get synchronized capturecompare input.
Definition: timer_a.c:190
uint16_t compareOutputMode
Definition: timer_a.h:281
uint16_t timerInterruptEnable_TAIE
Definition: timer_a.h:149
void Timer_A_initCompareMode(uint16_t baseAddress, Timer_A_initCompareModeParam *param)
Initializes Compare Mode.
Definition: timer_a.c:130
uint16_t dutyCycle
Specifies the dutycycle for the generated waveform.
Definition: timer_a.h:206
bool startTimer
Whether to start the timer immediately.
Definition: timer_a.h:249
uint16_t timerClear
Definition: timer_a.h:160
uint16_t captureCompareInterruptEnable_CCR0_CCIE
Definition: timer_a.h:154
uint16_t compareInterruptEnable
Definition: timer_a.h:270
uint16_t timerPeriod
Definition: timer_a.h:231
void Timer_A_setOutputForOutputModeOutBitValue(uint16_t baseAddress, uint16_t captureCompareRegister, uint8_t outputModeOutBitValue)
Set output bit for output mode.
Definition: timer_a.c:223
uint16_t clockSourceDivider
Definition: timer_a.h:228
Used in the Timer_A_initCaptureMode() function as the param parameter.
Definition: timer_a.h:77
Used in the Timer_A_initUpMode() function as the param parameter.
Definition: timer_a.h:214
Used in the Timer_A_initCompareMode() function as the param parameter.
Definition: timer_a.h:258
void Timer_A_enableCaptureCompareInterrupt(uint16_t baseAddress, uint16_t captureCompareRegister)
Enable capture compare interrupt.
Definition: timer_a.c:162
uint16_t captureMode
Definition: timer_a.h:91
void Timer_A_disableInterrupt(uint16_t baseAddress)
Disable timer interrupt.
Definition: timer_a.c:152
void Timer_A_initUpDownMode(uint16_t baseAddress, Timer_A_initUpDownModeParam *param)
Configures Timer_A in up down mode.
Definition: timer_a.c:79
uint16_t clockSource
Definition: timer_a.h:177
uint16_t compareValue
Is the count to be compared with in compare mode.
Definition: timer_a.h:283
uint16_t captureInputSelect
Definition: timer_a.h:98
void Timer_A_setCompareValue(uint16_t baseAddress, uint16_t compareRegister, uint16_t compareValue)
Sets the value of the capture-compare register.
Definition: timer_a.c:261
void Timer_A_initCaptureMode(uint16_t baseAddress, Timer_A_initCaptureModeParam *param)
Initializes Capture Mode.
Definition: timer_a.c:108
uint16_t Timer_A_getCounterValue(uint16_t baseAddress)
Reads the current timer count value.
Definition: timer_a.c:281
uint32_t Timer_A_getInterruptStatus(uint16_t baseAddress)
Get timer interrupt status.
Definition: timer_a.c:157
Used in the Timer_A_outputPWM() function as the param parameter.
Definition: timer_a.h:170
void Timer_A_outputPWM(uint16_t baseAddress, Timer_A_outputPWMParam *param)
Generate a PWM with timer running in up mode.
Definition: timer_a.c:233
uint16_t compareRegister
Definition: timer_a.h:265
uint16_t timerInterruptEnable_TAIE
Definition: timer_a.h:236
void Timer_A_initUpMode(uint16_t baseAddress, Timer_A_initUpModeParam *param)
Configures Timer_A in up mode.
Definition: timer_a.c:49
bool startTimer
Whether to start the timer immediately.
Definition: timer_a.h:162
uint16_t clockSourceDivider
Definition: timer_a.h:55
uint32_t Timer_A_getCaptureCompareInterruptStatus(uint16_t baseAddress, uint16_t captureCompareRegister, uint16_t mask)
Return capture compare interrupt status.
Definition: timer_a.c:176
uint16_t clockSource
Definition: timer_a.h:135
uint8_t Timer_A_getOutputForOutputModeOutBitValue(uint16_t baseAddress, uint16_t captureCompareRegister)
Get output bit for output mode.
Definition: timer_a.c:203
uint16_t clockSourceDivider
Definition: timer_a.h:142
Used in the Timer_A_initContinuousMode() function as the param parameter.
Definition: timer_a.h:41
uint16_t compareRegister
Definition: timer_a.h:193
void Timer_A_clear(uint16_t baseAddress)
Reset/Clear the timer clock divider, count direction, count.
Definition: timer_a.c:184
uint16_t captureInterruptEnable
Definition: timer_a.h:108
uint16_t timerPeriod
Selects the desired timer period.
Definition: timer_a.h:186
uint16_t timerInterruptEnable_TAIE
Definition: timer_a.h:60
uint16_t captureCompareInterruptEnable_CCR0_CCIE
Definition: timer_a.h:241
uint16_t clockSource
Definition: timer_a.h:221