31 #define PSS_KEY_VALUE PSS_KEY_KEY_VAL
33 #define PSS_SVSMH PSS_IE_SVSMHIE
35 #define PSS_FULL_PERFORMANCE_MODE 0x01
36 #define PSS_NORMAL_PERFORMANCE_MODE 0x00
uint_fast8_t PSS_getHighSidePerformanceMode(void)
Definition: pss.c:94
void PSS_clearInterruptFlag(void)
Definition: pss.c:157
void PSS_enableForcedDCDCOperation(void)
Definition: pss.c:21
void PSS_disableHighSidePinToggle(void)
Definition: pss.c:55
void PSS_registerInterrupt(void(*intHandler)(void))
Definition: pss.c:164
void PSS_disableInterrupt(void)
Definition: pss.c:145
void PSS_disableHighSideMonitor(void)
Definition: pss.c:111
uint32_t PSS_getInterruptStatus(void)
Definition: pss.c:152
uint_fast8_t PSS_getHighSideVoltageTrigger(void)
Definition: pss.c:132
void PSS_setHighSidePerformanceMode(uint_fast8_t powerMode)
Definition: pss.c:82
void PSS_disableForcedDCDCOperation(void)
Definition: pss.c:30
void PSS_enableHighSideMonitor(void)
Definition: pss.c:102
void PSS_setHighSideVoltageTrigger(uint_fast8_t triggerVoltage)
Definition: pss.c:120
void PSS_unregisterInterrupt(void)
Definition: pss.c:177
void PSS_enableHighSidePinToggle(bool activeLow)
Definition: pss.c:40
void PSS_enableInterrupt(void)
Definition: pss.c:138
void PSS_disableHighSide(void)
Definition: pss.c:73
void PSS_enableHighSide(void)
Definition: pss.c:64