31 #define PMAP_ENABLE_RECONFIGURATION PMAP_CTL_PRECFG
32 #define PMAP_DISABLE_RECONFIGURATION 0x00
40 #define PMAP_P1MAP ((uint32_t)P1MAP - PMAP_BASE)
41 #define PMAP_P2MAP ((uint32_t)P2MAP - PMAP_BASE)
42 #define PMAP_P3MAP ((uint32_t)P3MAP - PMAP_BASE)
43 #define PMAP_P4MAP ((uint32_t)P4MAP - PMAP_BASE)
44 #define PMAP_P5MAP ((uint32_t)P5MAP - PMAP_BASE)
45 #define PMAP_P6MAP ((uint32_t)P6MAP - PMAP_BASE)
46 #define PMAP_P7MAP ((uint32_t)P7MAP - PMAP_BASE)
72 uint8_t numberOfPorts, uint8_t portMapReconfigure);
75 #define PMAP_configurePortsMultipleInstance(a,b,c,d,e) PMAP_configurePorts(b,c,d,e)
void PMAP_configurePorts(const uint8_t *portMapping, uint8_t pxMAPy, uint8_t numberOfPorts, uint8_t portMapReconfigure)
Definition: pmap.c:5