Main Page
Modules
Data Structures
Files
Related Pages
File List
Globals
cygdrive
c
msp432-driverlib
src
driverlib
MSP432P4xx
debug.h
Go to the documentation of this file.
1
#ifndef __DEBUG_H__
2
#define __DEBUG_H__
3
4
//*****************************************************************************
5
//
6
// Prototype for the function that is called when an invalid argument is passed
7
// to an API. This is only used when doing a DEBUG build.
8
//
9
//*****************************************************************************
10
extern
void
__error__
(
char
*pcFilename,
unsigned
long
line);
11
12
//*****************************************************************************
13
//
14
// The ASSERT macro, which does the actual assertion checking. Typically, this
15
// will be for procedure arguments.
16
//
17
//*****************************************************************************
18
#ifdef DEBUG
19
#define ASSERT(expr) { \
20
if(!(expr)) \
21
{ \
22
__error__(__FILE__, __LINE__); \
23
} \
24
}
25
#else
26
#define ASSERT(expr)
27
#endif
28
29
#ifdef DEBUG
30
#define assert(expr) { \
31
if(!(expr)) \
32
{ \
33
__error__(__FILE__, __LINE__); \
34
} \
35
}
36
#else
37
#define assert(expr)
38
#endif
39
40
#endif // __DEBUG_H__
__error__
void __error__(char *pcFilename, unsigned long line)
Copyright 2015, Texas Instruments Incorporated