MSP430 IEC60730 Software Package 1.10.00.04
Release Notes
Document Revision: 032816.1603
This document is divided into the following sections:
- Updated MSP430 driver library to version 2.21.00.08
- Added support for MSP430FR26xx, MSP430FR25xx and MSP430FR2433
-
Modified CPU test for IAR and CCS
-
Devices with CPUX can now use small or large memory model
compiler option.
1.04.00.05
- Updated MSP430 driver library to version 2.00.00.16
- Updated CCS project spec file to use unix style directory path
1.03.00.01
- Added example project for DRV91670 device
- In this example IEC 60730 class B function have been implemented on a DC brushless motor control application using DRV91670
- IMPORTANT: Please refer to DRV91670 README file for more information regarding CCS support files for DRV91670.
1.02.00.6
- Updated CCS project to use projecspec file. Using projectspec file the file in example project are copy to the workspace instead of linked
- IEC60730 Configuration Tool can now be launch from CCS TI resource explorer
- User's Guide was updated to include Detailed information contained in API Guide
1.01.00.17
- Added support for MSP430FR57xx devices.
- Added CCS and IAR IEC60730_msp430fr5739_example
- Added MSP430 Software Package Configuration Tool.- The tool
can be found under "{IEC60730_PATH}\utils\" for more
information on how to use the tool please consult the
MSP430 IEC60730 Software Package Users Guide
- Added macro definitions in "IEC60730_user_config.h" for easy way to configure
Oscillator test to use different Timer_A module available in the device
- Bug Fixes for CPU and Oscillator test.
MSP430 IEC60730 Software Package can be installed as part of MSP430ware Driver Library or it can be use as a
stand alone library.
This release supports installation and development on
Microsoft Windows XP Workstations.
- MSP430 IEC60730 Software Package Dependencies:
- MSP430 IEC60730 Software Package Dependencies for MSP430FR26xx,
MSP430FR25xx and MSP430FR2433:
This release supports the following devices:
- MSP430G23xx
- MSP430G24xx
- MSP430G25xx
- MSP430G2x44
- MSP430G2x77
- MSP430F5xx
- MSP430FR57xx
- DRV91670
- MSP430FR26xx
- MSP430FR25xx
- MSP430FR2433
This release is a minor release version and has been tested.
The examples can be found in MSP430 IEC60730 Software Package Example Projects. The directory
contains five examples:
- IEC60730_emptyProject
- IEC60730_msp430f5529_example
- IEC60730_msp430g2553_example
- IEC60730_msp430fr5739_example
- IEC60730_msp430fr2633_example
For CCS, the examples can be imported using the import wizard.
For IAR, double click on the .eww file inside the IAR directory of each example project.
Please consult the
MSP430 IEC60730 Software Package Users Guide
for detailed instructions on how to to run the examples.
This is build 1.10.00.04 of MSP430 IEC60730 Software Package.
Support
Additional Resources
For more information, visit www.ti.com.