Texas Instruments

MSP430 IEC60730 Software Package  1.04.00.05

Release Notes 

Document Revision: 021215.1821

Introduction

This document is divided into the following sections:

Documentation

What's New

Revision History

1.03.00.01
1.02.00.6
1.01.00.17

Installation and Usage

MSP430 IEC60730 Software Package can be installed as part of MSP430ware Driver Library or it can be use as a stand alone library.

Host Support

This release supports installation and development on Microsoft Windows XP Workstations.

Dependencies

Device Support

This release supports the following devices:

Validation Information

This release is a minor release version and has been tested.

Examples

The examples can be found in MSP430 IEC60730 Software Package Example Projects. The directory contains four examples:

For CCS, the examples can be imported using the import wizard.

For IAR, double click on the .eww file inside the IAR directory of each example project.

Please consult the MSP430 IEC60730 Software Package Users Guide for detailed instructions on how to to run the examples.

Versioning

This is build 1.04.00.05 of  MSP430 IEC60730 Software Package.

Technical Support and Product Updates

Support

Additional Resources

For more information, visit www.ti.com.