Document Revision: 031815.1024
This is the MSP430™ PMBus Library.
The MSP430™ PMBus Library is a royalty-free set of API's that provide support for master protocols in a PMBus communication system.
This document is divided into the following sections:
The PMBus Library contains the following components.
doc | API Guide, Users Guide, and Examples Guide |
smbuslib | MSP430™ SMBus library required for communcations |
src | Library source code |
examples | Example projects |
N/A
This release supports installation and development on Microsoft Windows Workstations.
This release is a GA version.
The examples may be built with either IAR or CCS. To build the examples navigate to example folder, select a project and
click the .eww project files for IAR or import the .projectspec file for CCS. See the PMBus Users Guide for detailed usage instructions.
Current supported experimenters boards are found in the Device Support section of the release notes.
This is build 1.00.00.00 of MSP430™ PMBus Library
For more information, visit www.ti.com.