FlowESI GUI
1.20.00.00
|
To import CCS project generated by FlowESI GUI follow the next instructions:
To open an IAR project generated by FlowESI GUI follow the next instructions:
Once the projects have been imported/opened in CCS or IAR. Compile and load the code to the target. Running the code is dependent on the selections made in the "Output Selection" tab. The main difference between generated codes is way that auto calibration routines are initiated.
IMPORTANT: Selecting "Enable target communication via HID/UART communication bridge" will require the user to use the "Target Comm" panel in Flow ESI to start the auto calibration routines. If you are running the application on a linux platform, please see this note.
In order to start detecting rotation the application must perform the following tasks:
Depending on the output selection the calibration routines will let the user know the calibration process is complete using different methods. The table below shows the notification available for every output selection.
Output Option | Calibration type | Calibration Done notification |
---|---|---|
Toggle LED every time a rotation is detected | Auto calibrate TSM delay | Rotation LED is turn ON when TSM calibration is DONE |
Auto calibrate DAC thresholds | Rotation LED is turn OFF when DAC calibration is DONE | |
Display Rotation on LCD | Auto calibrate TSM delay | LCD displays "8888" when TSM calibration is DONE |
Auto calibrate DAC thresholds | LCD displays "0" when DAC calibration is DONE | |
Enable target communication via HID/UART communication bridge | Auto calibrate TSM delay | In "Target Comm" tab under "Sensor Calibration" Time State Machine calibration button will turn green and TSM delays will be displayed |
Auto calibrate DAC thresholds | In "Target Comm" tab under "Sensor Calibration" Digital to Analog Converter (DAC) calibration button will turn green and DAC thresholds will be displayed |
To start auto calibration using "Target Comm" panel follow these steps: